PRECISION THERMOCOUPLE AMPLIFIERS WITH INTEGRATED COLD JUNCTION COMPENSATION PROVIDE ACCURATE TEMPERATURE MEASUREMENT

- Analog Devices Announces Series of Low-cost Precision Thermocouple Amplifiers.
ADI introduces a series of precision thermocouple amplifiers for K- and J-type thermocouples.

Norwood, MA (05/26/2010) - Analog Devices, Inc. (ADI), a world leader in semiconductors for mixed-signal processing applications and leading supplier of signal conditioning technology, today introduced a series of low-cost, precision thermocouple amplifiers for K- and J-type thermocouples, which are widely used to measure temperature in industrial, commercial, and scientific applications.

Thermocouple systems provide accurate and reliable temperature measurements and control, are cost-effective, and can measure a wide range of temperatures. However, to achieve good measurement performance cold junction compensation and a high gain accuracy precision amplifier are required. Analog Devices’ AD8494, AD8495, AD8496 and AD8497 thermocouple amplifiers address this issue by featuring on-chip cold junction compensation that automatically adjusts the thermocouple output for changes in ambient temperature. This feature greatly simplifies the design process and reduces system cost relative to similar discrete solutions. For more information, visit http://www.analog.com/pr/AD8495.

“We’re using ADI’s thermocouple amplifiers in designs for ultra-pure heating controllers for industrial applications,” said Bob Woskow, president, Robert Marshall and Associates, an Encino, California-based embedded microcontroller design and development consultancy. “ADI’s amplifiers are smaller, complete with internal cold junction compensation and thus are quite simple to use with few or no additional parts needed on the printed circuit board. They will do everything we need a thermocouple amplifier to do.”

The four new precision thermocouple amplifiers each convert the small voltages generated by a thermocouple junction into a 5 mV/°C analog signal that can easily be read by an ADC (analog-to-digital converter) or microcontroller. The integrated cold junction compensation ensures accurate measurement over a wide range of ambient temperatures while the high common-mode rejection (0.1°C/V) allows the AD849x to reject common-mode noise that may be associated with long lead thermocouples. The AD849x thermocouple amplifiers operate off a wide variety of voltages, from single 2.7-V to dual ±18-V supplies and are very power efficient, consuming only 180 uA quiescent supply current. In single-supply operation the amplifiers can directly interface to lower-supply ADCs while higher, dual-supply voltages can be used for industrial systems that require a wide common mode input range. With a single 5-V supply, the AD849x amplifiers can cover nearly 1,000-degrees of a thermocouple’s temperature range. A reference pin allows for level shifting of the 0°C output so that negative temperatures can easily be measured, even on a single supply.

“Temperature is the second most measured parameter. Systems using ADI’s linear products provide rugged, repeatable temperature sensing with simplified design,” said Steve Sockolov, director, Precision Signal Conditioning Group, Analog Devices. “Integrated cold junction compensation greatly simplifies thermocouple system design for use in all applications including medical dialysis machines, blood analyzers, process control and instrumentation.”

Thermocouple Amplifier Key Features and Benefits

  • Integrated cold junction compensation
  • 5-mV/°C output with single-supply operation down to 2.7 V and rail-to-rail output
  • High-impedance differential input
  • Reference pin allows offset adjustment
  • Wide power-supply range: 2.7 V to ±18 V
  • High Gain Accuracy – 0.1%
  • Low power: 180 µA quiescent supply current
  • Low cost: less than US$1.00, in volume
  • Lead-free MSOP-8 package

Availability, Pricing and Complementary Products

Product Sample
Availability
Thermocouple
Type
Range
Reference
Junction
Price Each
Per 10K
Packaging
AD8494 NOW J-Type 0°C - 50°C $0.98 8-lead MSOP
AD8495 NOW K-Type 0°C - 50°C $0.98 8-lead MSOP
AD8496 NOW J-Type 25°C - 100°C $0.98 8-lead MSOP
AD8497 NOW K-Type 25°C - 100°C $0.98 8-lead MSOP
As part of a signal chain, the AD8494/5/6/7 thermocouple amplifiers work well with ADI’s precision data converters, such as AD7685, and reference buffer amplifiers, such as ADI’s AD8607.

More Information and Samples

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Subscribe to ADI’s News Feed.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

Editor's Contact Information:

Bob Olson
791/937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close