myAnalog_id
https://my.analog.com
https://registration.analog.com
Analog Devices
  • View Cart
  • myAnalog
  • Log In
  • Contact ADI
  • Parametric Search
  • Replacement Parts Search
  • ADI Home
  •  >Interface
  •  >Digital Isolators
  •  >ADUM1300
  • Save to myAnalog  
  • Print
  • Email this Page
  • Interface
  • Digital Isolators
  • Level Translators
  • RS-232
  • RS-485
  • Transceivers
  • All Product Categories
  • All Applications
  • Design Tools & Support
  • Buy Online


iCoupler® Products with isoPower™ Technology:
Signal and Power Transfer across Isolation Barrier
Using Micro-Transformers

Baoxing Chen,
Analog Devices, Inc.

Download this White Paper
(pdf, 1,338,008 bytes)


Introduction


Isolation between circuit components is typically required for safety and/or data integrity considerations. For example, isolation protects sensitive circuit components and human interface on the system side from dangerous voltage levels present on the field side, where more robust components such as sensors and actuators reside. Isolation can also eliminate common mode noises or ground loops that affect data acquisition accuracy. While data transfer across an isolation barrier can be achieved through traditional opto-couplers or Analog Devices' iCouplers, the main challenge and common headache has been to find a way to transmit power from the non-isolated system side to the isolated field side. This paper discusses the technology behind a new approach addresses this challenge by integrating power supply isolation with data signal isolation using Analog Devices' latest iCoupler products.


Until recently, transferring power across an isolation barrier required either a separate DC/DC converter, which is relatively large, expensive and has insufficient isolation, or a custom discrete approach, which is not only bulky but also difficult to design and interface. These approaches have been the only viable alternatives, even in applications such as data acquisition modules where only small levels of isolated power are needed.


Analog Devices has recently addressed this issue with the introduction of a complete and fully integrated isolation solution involving signal and power transfer across an isolation barrier using micro-transformers. This extension to our iCoupler technology, termed isoPower, is a breakthrough alternative. Signal and power within a single component, eliminates the need for a bulky, expensive, difficult to design isolated power supply and provides adequate isolation up to 5kV. It can significantly reduce the total isolation system cost, the board space and design time. A two channel iCoupler device with isoPower as shown in Figure 1 is almost 90% smaller and 70% less expensive.

Cost and Comparison
Figure 1: Cost and Size Comparison Between Traditional Approach and isoPower Approach


back to top



iCoupler Technology with isoPower


The integration of DC/DC converters involves the use of transformer switches, rectification diodes and most importantly, a transformer. Reducing the size of the transformer to enable its integration in a complete isolation solution is made possible by using high switching frequencies, on the order of 300 MHz. This runs counter to the approach used in magnetic core transformers where the permeability of the magnetic core starts to degrade at high frequencies, leading to appreciable core loss that lowers efficiency. In addition, a magnetic core could also compromise the isolation rating of the transformers. Coreless iCoupler transformers, on the other hand, can be switched at higher frequencies and are much simpler to implement.


The micro-transformers used in iCoupler devices are built on top of a CMOS substrate. Figure 2 shows a cross-section of the isolated transformer structure, and Figure 3 is a die photo with both power and signal transformers. The transformer series resistance is minimized through the use of 6µm thick plated Au for both the primary and the secondary spirals. The 20µm thick polyimide in between the primary and the secondary provides HV isolation up to 5KV. The additional 5µm thick polyimide under the bottom spiral helps to reduce substrate capacitance and substrate loss. The substrate loss is further reduced through careful designed patterned ground shield using available underlying IC metal. The proximity effect and eddy current loss is less of a concern for the stacked transformers with large magnetic coupling coefficient. The design of the coils can be done through the optimization of coil parameters, such as the number of turns, trace width and trace pitch. The quality factor (Q) at 300MHz can be as high as 20 for the top coil and 15 for the bottom coil. The high Q for the micro-transformer structure makes an efficient power transfer possible.

Cross Section
Figure 2: Cross Section of iCoupler Transformer Coil

Transformer Die
Figure 3: Photograph of Transformer Die Showing the Power
Transformer Coil and the Two Data Transformer Coils.


The transfer of the digital signal is realized through transmitting short pulses around 1nS wide across the transformers with two consecutive short pulses to indicate a leading edge and a single short pulse as a falling edge. Figure 4 shows the signal transfer block diagram. A non-retriggerable mono-stable at the secondary generates detection pulses. If two pulses are detected, the output is set to High. On the other hand, if a single pulse is detected, the output is set to Low. An input filter helps to increase noise immunity. The DC correctness is guaranteed by refresh signals sent into the transformers when no signal edges are detected for about 1µS. If the input is high, two consecutive short pulses are generated as refresh pulses and if the input is low, refresh of a single short pulse is generated. To complement the refresh circuit on the driver side, a watchdog is implemented in the receiver to make sure the output is at a fail-safe state when no refresh pulses are detected.

Digital Signal Transfer Block Diagram
Figure 4: Digital Signal Transfer Block Diagram


Similar micro-transformers are used to transfer power. Because of their small L/R ratio, the transformers need to be switched at a high frequency to avoid current saturation and to achieve high efficiency. An example of four complimentary CMOS switches implemented in a cross-coupled configuration together with the transformer forming sustaining oscillation is shown in Figure 5. The tank component sizes are optimized to maximize the energy transfer efficiency. The integrated Schottky diodes were used as rectification devices. These diodes turn on and recover fast enough for 300MHz rectification. The diodes need to be sized such that they stay in Schottky region during rectification. A linear regulator on the secondary maintains the output voltage with output load or input supply variations. Efficiency is less of concern for many low power applications. To improve efficiency and maintain energy regulation, an optional feedback signal transformer can be added. The feedback signal would turn on/off the LC tank instead of controlling the transformer switches directly. This approach essentially separates the energy regulation from energy conversion allowing optimized power transfer and maintaining regulation.

Digital Signal Transfer Block Diagram
Figure 5: Power Transfer Block Diagram

One common concern about switching transformers is their electromagnetic interference, particularly for a transformer switching at 300MHz. Using the far-field approximation,


P=160 π6I2Σ(rn/λ)4; n = 1,2,...,N
where: P = total radiated power
I = coil loop current


The wavelength, λ at 300MHz is about 1 meter, the transformer with a radius in the range of 0.5mm is still a very poor antenna with a small r/λ. It is estimated that the total radiated power is still less than 500pW even if the part is operating at 300MHz with a loop current of 350mA. The near field radiation drops rapidly with the distance from the transformer. The on-chip transformers are only closely coupled with a small separation, 20µm in our case.


back to top




Example Application: The ADuM5242 in a Secondary Control Power Supply


Secondary control architectures have gained traction as new power supplies trend toward lower supply voltage, faster dynamic response and more system interaction between the supply and the load. There are two main difficulties in adopting secondary control versus primary control. The first is the need of high performance digital isolation versus analog isolation. An inexpensive analog opto-coupler is typically used to send analog feedback error signal from the secondary to the primary in a system with primary control while an expensive or bulky digital coupler would be needed to send PWM signals across the isolation barrier for a system with secondary control.


The second difficulty is the need for power at the secondary controller before the system has started up. The primary controller has no such issue as power is always available at the primary side. There are mainly two ways to solve this secondary control start-up issue. One method is to add an auxiliary power supply exclusively for the secondary controller start-up. A second method is to have a dedicated start-up component on the primary side to build initial bias at the secondary for the start up of secondary controller.


Analog Devices' ADuM5242, a dual channel digital isolator with a 50mW isolated output is an ideal solution to the startup problem. This 8-lead SOIC component provides two isolation channels that support PWM signals up to 10Mbps and 10 mA of 5V isolated power for the start up of the secondary controller. The user has further option to disable the power once the system is started up. The disable is achieved through monitoring the input supply voltage. When the input supply drops below 4V the feedback control switch shown in Figure 5 is turned off. Figure 6 is an example application block diagram for the use of ADuM5242 in a secondary control system. The two digital signal channels provide the feedback signals from the secondary controller with synchronous rectification to drive the half-bridge drivers at the primary.

Example of Secondary Control System
Figure 6: Example of Secondary Control System Employing ADuM5242 with isoPower

Together with ADuM5242, two other data channel configurations have also been introduced. The ADuM5240 has two isolated output channels while the ADuM5241 has one isolated output and one isolated input. This provides the flexibility to support a wide variety of applications. The ADuM524x products can also be used in combination with other multi-channel iCoupler devices to configure higher quantities of isolated signal channels.


back to top




Summary


iCoupler technology with isoPower provides a complete isolation solution within a single package. Not only does it offer state-of-the-art digital signal isolation having substantial advantages over opto-couplers in terms of power, size and performance, but it also eliminates the need for a separate, isolated power supply. The iCoupler technology provides unprecedented possibilities for functional integration that can dramatically reduce the complexity, size and total cost of the isolated systems.

back to top

  • Privacy/Security
  • myAnalog
  • Contact ADI
  • Site Map
  • Registration
  • Technical Support
  • Terms of Use
© 1995-2008 Analog Devices, Inc. All Rights Reserved