Norwood, MA (11/13/2012) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications and a pioneer in digital isolator technology, today introduced the industry’s smallest isolated DC-to-DC converters. The ADuM5010, ADuM6010, ADuM521x and ADuM621x use ADI’s proprietary isoPower® isolated DC-to-DC converter technology to deliver 150 mW of output power while using less board space than competing module-based solutions. The ADuM521x and ADuM621x also integrate two channels of ADI’s award winning iCoupler® data isolation technology to reduce board space by up to 75 percent compared to optocoupler-based alternatives. The converters expand ADI’s isolated power portfolio by providing designers with a compact, easy-to-implement, cost-effective approach to meeting both isolated power and data requirements. The combination of size and output power also addresses the growing space and power constraints engineers must consider when designing control systems, test and measurement equipment, power supplies, motor drives, and other industrial and instrumentation applications.
"This new line of isoPower DC-to-DC converters delivers an excellent balance between power and size that will allow customers to design more functionality and efficiency into smaller form factors while continuing to minimize system cost," said David Krakauer, product line manager, iCoupler Digital Isolator Products, Analog Devices. "ADI’s collaborative approach, design support and system-level knowledge help our customers take full advantage of our power isolation technology."
All of the new DC-to-DC converters provide regulated, isolated power, adjustable between 3.15 V and 5.25 V. The ADuM5010 and ADuM521x are certified for 2.5-kV rms (1-minute) isolation, while the ADuM6010 and ADuM621x are certified for 3.75-kV rms (1-minute) isolation with further certification for reinforced insulation per VDE 0884-10. By incorporating ADI’s iCoupler digital isolator technology, the ADuM521x and ADuM621x reduce component count and simplify and improve design speed, reliability, and efficiency by eliminating the need for optocouplers. Quad-channel versions of these products using ADI’s smaller, lower cost isoPower technology are forthcoming.
Analog Devices pre-certifies its converter modules to help designers reduce system development time, unlike multi-component discrete DC-to-DC converters, which require that designers undertake the costly and time consuming process of individually certifying a dozen or more parts. Additionally, ADI’s isolated DC-to-DC converter modules require no added components aside from two bypass capacitors, easing design complexity and reducing time to market.
Catalog distributors Digi-Key Corp. and Premier Farnell plc are stocking inventory of both silicon and evaluation boards.
| Product | Sample Availability | 2-Channel iCoupler Digital Isolation Core | Price per 1k units | Packaging |
|---|---|---|---|---|
| ADuM5010 | Now | - | $1.54 | 20-lead SSOP |
| ADuM6010 | Now | - | $2.24 | 20-lead SSOP |
| ADuM5210 | Now | Yes | $2.32 | 20-lead SSOP |
| ADuM5211 | Now | Yes | $2.32 | 20-lead SSOP |
| ADuM5211 | Now | Yes | $2.32 | 20-lead SSOP |
| ADuM5212 | Now | Yes | $3.32 | 20-lead SSOP |
| ADuM6210 | Now | Yes | $3.36 | 20-lead SSOP |
| ADuM6211 | Now | Yes | $3.36 | 20-lead SSOP |
| ADuM6212 | Now | Yes | $3.36 | 20-lead SSOP |
| EVAL-ADUM5010EBZ Evaluation Board | Now | $59.00 each | - | |
| EVAL-ADUM5210EBZ 2 channel Evaluation Board | Now | $69.00 each | - |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
iCoupler and isoPower are registered trademarks of Analog Devices, Inc. All other trademarks are the property of their respective owners.
Joe Dussi
781-937-1216
joe.dussi@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved