ANALOG DEVICES INTRODUCES INDUSTRY'S SMALLEST ISOLATED DC-TO-DC CONVERTER

New iCoupler® digital isolation device with isoPower® dc-to-dc converter technology delivers 50 percent reduction in size and cost compared to optocoupler-based solutions.

Norwood, MA (12/16/2010) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, is expanding its extensive portfolio of digital isolation products with the industry's smallest isolated dc-to-dc converter. Offering a 5-kV rms (root-mean square) isolation rating in a 10-mm x 10-mm package, the ADuM6000 is a 0.5 watt device that integrates ADI's proprietary iCoupler digital isolation technology and isoPower dc-to-dc converter. The new digital isolator allows designers to free up valuable circuit-board real estate while eliminating the time-consuming step of securing medical or other safety approvals (such as IEC-60601-1), all at a fraction of the cost of alternative devices, including optocouplers. Safety is a key requirement in medical and industrial designs, and the ADuM6000 protects the device and end users from exposure to voltage levels that could compromise safety and reliability. Watch a video on the ADuM6000 digital isolators.

The ADuM6000 digital isolator enables designers to reduce the form factor of their system module or to maintain the same form factor even as they add more features and functions. With alternate solutions, such as optocouplers and separate, isolated dc-to-dc converters, it may not be possible to add new functionality to existing system modules.

Also now available are the ADuM620x series of dual-channel digital isolators that feature isoPower integrated, isolated dc-to-dc converter technology and 5-kV rms isolation rating. The ADuM620x series includes the ADuM6200, ADuM6201 and ADuM6202 digital isolation products that differ by channel configuration.

Availability, Pricing and Complementary Components

Product Availability Price Each per 1,000 Channel Configuration Package
ADuM6000 Now $3.96 - 16-lead SOIC
ADuM6200 Now $5.12 2/0 16-lead SOIC
ADuM6201 Now $5.12 1/1 16-lead SOIC
ADuM6202 Now $5.12 0/2 16-lead SOIC

In some designs requiring USB (universal serial bus) isolation and isolated power, the ADuM4160 USB isolator can be used together with the ADuM6xxx devices.

iCoupler® Technology

With more than 450 million channels deployed throughout the industry, ADI's proven iCoupler technology is based on chip-scale transformers, rather than the LEDs and photodiodes used in optocouplers. Transformers can support higher data rates and lower power consumption, and are more stable over life as compared to LEDs and photodiodes. By fabricating the transformers directly on-chip using wafer-level processing, iCoupler channels can be integrated with each other and other semiconductor functions at low cost. iCoupler transformers are planar structures formed from CMOS and gold metal layers. A high breakdown polyimide layer underneath the gold layer insulates the top transformer coil from the bottom. CMOS circuits connected to the top coil and bottom coil provide the interface between each transformer and its external signals. For more on ADI's iCoupler digital isolation technology, visit: www.analog.com/icoupler.

isoPower® DC-to-DC Converter

ADI's isoPower integrated, isolated dc-to-dc converter uses the same chip-scale transformer technology, but instead of transmitting data, isoPower employs switches, rectifiers, and regulators to generate power that is isolated to the same degree as the data channels.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

iCoupler and isoPower are registered trademarks of Analog Devices, Inc. All other trademarks are the property of their respective owners.

Follow ADI on Twitter at http://www.twitter.com/ADI_News

Editor's Contact Information:

Linda Kincaid
(781)937-1472

linda.kincaid@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close