Norwood, MA (09/28/2011) - Analog Devices, Inc. (ADI) today unveiled a series of high-speed amplifiers that establish a new performance standard with the best combination of high-speed, low noise and low power. Designed for portable, multi-channel and low power instrumentation and healthcare equipment, the ADA4896-2 (dual), ADA4897-1(single) and ADA4897-2 (dual) high-speed amplifiers provide the highest large-signal bandwidth and slew rate with the lowest noise available today in a rail-to-rail amplifier under 10 mW. Each amplifier features low noise of 1 nV/√Hz and 120-V/µs slew rate while consuming only 3 mA of supply current. Further, the 1/f noise @10Hz is a low 2.4 nV/√Hz. Watch this video and learn more about ADI's new series of high-speed amplifiers.
Also announced as part of this high-speed amplifier series was the ADA4895-2 dual de-compensated high-speed amplifier. It delivers 1.5-GHz gain-bandwidth product at gains of +10 and greater, making it ideal as a high-speed, high-gain pre-amplifier.
The new rail-to-rail amplifiers operate across the extended industrial temperature range of -40˚C to +125˚C and offer a 3-V to 10-V supply range. The ADA4895-2 and ADA4897-1/ -2 include an output disable feature.
| Product | Features | Availability | Price Each Per 1,000 | Packaging |
|---|---|---|---|---|
| ADA4897-1 | Single, Disable | Full Volume Production | $1.89 | 8-lead SOIC 6-lead SOT |
| ADA4897-2 | Dual, Disable | Samples Now | $3.20 | 10-lead MSOP |
| ADA4896-2 | Dual | Full Volume Production | $3.20 | 8-lead LFCSP 8-lead MSOP |
| ADA4895-2 | Dual, Disable (Gain ≥+10) | Samples Now | $3.20 | 10-lead MSOP |
Complementary components for these amplifiers include the AD7982 18-bit A/D converter and the AD9279 octal (eight-channel) ultrasound receivers. Find additional high-speed low noise amplifiers at http://www.analog.com/en/high-speed-op-amps/low-noise-low-distortion-amplifiers/products/index.html.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
To subscribe to ADI's News Feed http://www.analog.com/en/homepage/news.xml
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue/
Bob Olson
781-937-1666
bob.olson@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved