| Asynchronous Sample Rate Converter (ASRC) |
Audio Post Decoders |
1.0.0 |
Sep-09 |
Asynchronous Sample Rate Converter (ASRC) is used for audio sampling rate conversion in both consumer and professional applications. The ASRC software module supports a variety of sample rate configurations. The ASRC software module can be used to change the sampling frequency in small steps which vary with time without producing any audible artifacts in the output, during the change. Such a time ...more
| Download Production Code |
| Dolby® Advanced Fader |
Audio Decoders and Post Decoders |
1.1.0 |
Oct-09 |
Dolby® Advanced Fader & Mixer is one of the central components in the Dolby Automotive Entertainment Program (DAEP) Post-Processing System. The DAEP system is aimed at improving the in-car listening experience by taking into consideration the positions and directionality of the listener with respect to the available speaker sets. The Dolby Advanced Fader Mixer provides audio channel ...more
| Request Evaluation Code Request Production Code |
| Dolby® Intelligent Mixer (eMix) |
Audio Decoders and Post Decoders |
3.1.0 |
Aug-09 |
Dolby® Intelligent Mixer is a sub component of the Dolby Car Audio system...more |
Request Evaluation Code Request Production Code |
| Dolby® Digital (AC-3) 5.1 Decoder |
Audio Decoders and Post Decoders |
3.0.0 |
Nov-09 |
The ADI Dolby® Digital (AC-3) 5.1 Decoder library for the SHARC processor is an implementation of a Dolby Digital Consumer Decoder, compliant with the Advanced Television...more |
Download Evaluation Code Request Production Code |
| Dolby® Digital EX Decoder |
Audio Decoder |
1.1.0 |
Dec-09 |
Dolby® Digital EX is an extension of the Dolby Digital decoding algorithm that adds a center rear channel or two back channels to 5.1 channel playback, expanding the surround sound experience to 6.1 channels...more |
Request Evaluation Code Request Production Code |
| Dolby® Headphone v2 |
Audio Decoders and Post Decoders |
2.3.0 |
Oct-09 |
Dolby® Headphone is a propriety algorithm from Dolby Laboratories intended for creating 5.1 realistic surround sound effects on headphones. The Dolby headphone technology is capable of processing 24 bit/96 Khz audio such as DVD-Audio from sources providing up to 7.1 channels. Dolby Headphone can also produce 5.1 surround effects from stereo sources when used in combination with Dolby Prologic...more |
Download Evaluation Code Request Production Code |
| Dolby® Pro Logic IIx |
Audio Decoders and Post Decoders |
3.2.0 |
Nov-09 |
Dolby® Pro Logic IIx is a proprietary algorithm from Dolby Laboratories intended for extending stereo or 5.1-channel audio to 6.1 or 7.1 channels. The Dolby Pro Logic IIx Decoder (DPLIIx) uses matrix surround decoding technology to create an extended-channel surround sound playback experience. DPLIIx has applications in home and car entertainment systems, PC audio, games consoles, and...more |
Download Evaluation Code Request Production Code |
| Dolby® Virtual Speaker |
Audio Decoders and Post Decoders |
2.3.0 |
Jul-09 |
DVS which is an acronym for Dolby® Virtual Speaker, which is a propriety algorithm from Dolby Labs intended for creating realistic 5.1 surround effects on two channel output...more |
Download Evaluation Code Request Production Code |
| DTS® 5.1 Decoder |
Audio Decoders and Post Decoders |
3.0.0 |
Dec-09 |
The DTS® technology as relevant from the name Digital Theatre Systems was initially focussed on providing high fidelity, full bandwidth, and multi channel surround sound...more |
Request Evaluation Code Request Production Code |
| DTS® Neo:6 Matrix Decoder |
Audio Decoders and Post Decoders |
2.3.0 |
Dec-09 |
Neo:6 is a DTS® propriety algorithm aimed with the primary objective of providing a richer and more natural sound in multi channel derived from a two channel source...more |
Request Evaluation Code Request Production Code |
| Neural Surround Decoder |
Audio Decoders and Post Decoders |
2.2.0 |
Jan-10 |
The DTS Neural Surround Decoder is an up mixing algorithm capable of producing 3.1, 4.1, 5.1, 6.1, and 7.1 surround sound from Neural Surround encoded stereo content. It is widely used ...more |
Request Evaluation Code Request Production Code |