content here.
content here.

Documentation Errata for ADSP-21362/ADSP-21363/ADSP-21364/ADSP-21365/ADSP-21366 SHARC Processors


Chapter: N/A Page: 12
Reference Number: 39473
Change
In table 4 (Pin Descriptions), in the State During and After Reset column, the state listed for the Flag 3-0 pins needs to change from:
Three-state

Change to:
Input

back to top


Chapter: N/A Page: 13
Reference Number: 35262
Change
In table 4, the "State During and After Reset" column describes the SPICLK and MOSI pins as "Three state with pull up enabled". This info is not completely accurate, because---when in SPI Master boot mode only---these pins are driven during and after reset. Add the following footnote to the "State During and After Reset" entries for these pins:
In SPI Master boot mode, the MOSI and SPICLK are driven during reset and after reset.

back to top


Chapter: N/A Page: 19
Reference Number: 36783
Change
Add the following to the paragraph in the "Power-Up Sequencing" section:
Note that during power-up, a leakage current of approximately 200μA may be observed on the RESET pin. This leakage current results from the weak internal pull-up resistor on this pin being enabled during power-up.

back to top


Last Updated: October 28, 2008