myAnalog_id
https://my.analog.com
https://registration.analog.com
Analog Devices
  • View Cart
  • myAnalog
  • Log In
  • Contact ADI
  • Parametric Search
  • Replacement Parts Search
  • ADI Home
  •  >Embedded Processing and DSP
  •  >Communities
  •  >DSP Community
  • Save to myAnalog  
  • Print
  • Email this Page
  • Communities
  • DSP Community
  • Embedded Processing Community
  • All Product Categories
  • All Applications
  • Design Tools & Support
  • Buy Online

Jerry McGuire

A Dynamic Power Play
June 2008

Jerry McGuire

The Personal Media Player is continuing to evolve. With its roots in the humble MP3 player that was considered revolutionary a few short years ago, feature sets are constantly being updated, and lines are continuing to be blurred between existing devices, such as telephones, navigation systems, media players, and computers, cameras and game consoles. Digital television, and wireless communication of all types from personal area and local area networks to satellite reception, to gestural user interfaces, are competing to be the ‘next big thing’ in the ultimate consumer handheld device. All of these developments point to even higher levels of processing performance, larger storage capacity, and greater power demand in a nearly fixed size device.

Many manufacturers are finding that the best design approach in such a dynamic market is to keep as much functionality as possible in software that targets a platform that hits the market requirements in terms of performance, price, size, and battery life. This approach reduces time to market and technical risk, while providing features that lead the competitive offerings. The avoidance, wherever possible, of fixed function hardware that can quickly become obsolete or irrelevant, and the use of a performance-scalable processor, provides a multi-product, multi-regional platform that reduces development time and risk as product cycles shrink and new features, media formats, and digital rights management schemes emerge.

“All of these developments point to even higher levels of processing performance, larger storage capacity, and greater power demand in a nearly fixed size device.”
The Chinese developer, Aigo, credits the Blackfin with shortening time to market and reducing technical and schedule risk in product design, since the inherent flexibility of a Blackfin platform allows for rapid development cycles. They also took advantage of the wealth of software that is available for Blackfin, and the ADI partners that are available to develop and customize complete solutions. Aigo could have selected other hardware platforms, (and has used others in the past) but has found that Blackfin processors provide the best combination of high performance, low power, peripheral and communication ports, pricing structure and a vital partner network.

The Blackfin product roadmap also provides a path for continuous improvement in these dimensions over time. Developers can start with one Blackfin part and move to others in the family as performance needs change or improvements in power management technology become available. We expect to see many power sensitive designs to incorporate the Blackfin BF52x parts due to their leadership in power efficiency and advanced power management. These are essential to building more functionality into battery-powered devices, such as personal media players.

Innovators in the consumer electronics field will undoubtedly continue to find that the Blackfin ‘sweet spot’ of power, performance, peripherals, price and partners is the place to look for solutions to address these opportunities. We can’t wait to see what happens next. It’s a good bet that a Blackfin will be at the center of it.

Jerry McGuire is a Vice President of Analog Devices' General Purpose DSP Group. His column appears here regularly.

  • Privacy/Security
  • myAnalog
  • Contact ADI
  • Site Map
  • Registration
  • Technical Support
  • Terms of Use
© 1995-2008 Analog Devices, Inc. All Rights Reserved