The new Blackfin processors - BF512, BF514, BF516, and BF518 - are taking convergent processing to a whole new level. More than DSPs, they're DSP and microcontroller together, with connectivity that's designed in. These single-core processors surpass outdated heterogeneous MCU and DSP approaches in every important way: reducing part count, system cost, board space, and power consumption. Like discrete DSPs, the BF51x processors feature high clock rates (up to 400 MHz/800 MMACS) and low power disapption per unit of processing (mW/MMACS), and like traditional MCUs, these new convergent processors are both OS - and compiler-friendly.

The new BF51x series are the future-proof processors that will help you reduce time to market, cost, and power consumption - while simplifying the design process at the same time. For a broad spectrum of portable, VoIP, and industrial applications, they're the highest performance, low power processors in the world. And they're another potent example of Analog Devices innovation at work.

Learn more about the BF51x Blackfin processors: