|
| Chapter: 1 |
Page: 2 |
| Reference Number: 34426 |
| Change |
In the "Supported Platforms" section, change the following text from: The following platforms are supported:- Windows 2000® SP4
- Windows XP® Professional SP2 (or greater)
- Windows Vista Business edition
- Windows Vista Enterprise edition
- Windows Vista Ultimate edition
Note: Windows NT®, Windows 98, and Windows ME are not supported. Note: VisualDSP++ 5.0 requires an Intel Pentium 32-bit processor (or x86 compatible) that is 1 GHz or faster. 64-bit host processors (x64) and 64-bit Windows editions are not supported. The VisualDSP++ License Manager is also supported on: Change the text to: VisualDSP++ is supported on the following platforms: - Windows 2000® SP4
- Windows XP® Professional SP2 (or greater)
- Windows Vista Business edition
- Windows Vista Enterprise edition
- Windows Vista Ultimate edition
System Requirements: VisualDSP++ 5.0 requires an Intel Pentium 32-bit processor (or x86 compatible) that is 1 GHz or faster, 512 MB RAM, 2GB available hard disk space, 1 open USB Port. Note: Windows NT®, Windows 98, and Windows ME are not supported. Note: 64-bit host processors (x64) and 64-bit Windows editions are not supported. The VisualDSP++ Floating License Server is also supported on: |
back to top |
|
| Chapter: 1 |
Page: 2 |
| Reference Number: 35997 |
| Change |
The LicenseAgreement.txt is not part of the VisualDSP++ 5.0 installation, so the reference to it should be removed from the License Guide. Change from: VisualDSP++ is provided under the terms of the VisualDSP++ Tools License Agreement. To view the full agreement, refer to the License Agreement.txt file located in the folder. Change to: VisualDSP++ is provided under the terms of the VisualDSP++ Tools License Agreement. The full agreement is presented to the user during installation of VisualDSP++, and a copy can be requested from processor.tools.support@analog.com. |
back to top |
|