content here.
content here.

Documentation Errata for ADSP-BF54x Blackfin Processor Hardware Reference (Volume 2 of 2) Preliminary, Revision 0.4, August 2008


Chapter:  16 Page: 4
Reference Number: 39360
Change
There are a number of minor typographic errors in chapter 16. These include:
  • Page 16-14: Says ADSO-54x instead of ADSP-54x
  • Page 16-17: Some of the parenthesis next to function names have an incorrect font (the normal one rather than the monospace font). This issue affects other pages also.
  • Page 16-20: Same font issue when talking about the arguments to the bfrom_OtpCommand()
  • Page 16-20: Should be OTP_INIT, not OTP_init
  • Page 16-21: Has OTP_PREV_WR_ERRO instead of OTP_PREV_WR_ERROR
  • Page 16-21 and 16-22: The text refers to &DATA = NULL", but nowhere else has DATA been declared or referred to. Instead, the text should read pPageContent or perhaps the third parameter.
  • Listing 16-4: The ssync does not match the ssync in listing 16-5
  • Listing 16-5: Listing has too many close parenthesis.

back to top


Last Updated: October 28, 2008