Rarely Asked Question Page

About The Author
David Buchanan ,
Product Applications Engineer Manager, Analog Devices

With no signal at the input to my ADC, why are the output data bits switching?

People unfamiliar with high-speed ADCs might expect a converter's digital output to be constant given a static analog input, but this is similar to expecting to see a simple dc offset error at the output of an op amp with no input signal. If you remove the input signal to an amplifier circuit and measure the output voltage with a DVM, the reading will tell you the amplifier's offset. The DVM is averaging the displayed results (using an ADC!), however, so it will not reveal the noise at the amplifier's output. Measuring the noise requires a scope or a spectrum analyzer.

Like any other component in the signal chain, ADCs have their own thermal noise contribution. Thus, if you want to verify that the ADC is behaving as expected with no input signal, you need to capture a block of data and average it, just as the DVM does with the amplifier circuit. High-speed ADCs typically float to their midscale code, plus or minus any inherent offset, so the resulting average output code should be within the ADC's offset specification. While analyzing the block of data you've captured, you can easily verify the noise performance of the ADC. The data sheet specification is input referred noise, which is specified in LSB rms. The measurement is known as a grounded input histogram test, although the nomenclature stems from early converters that had a bipolar input range centered on ground, so shorting the input to ground was equivalent to having no input signal. Modern high-speed converters typically operate with a single supply, so their input common-mode voltage is the midpoint of the front-end analog power supply rather than ground. Luckily for you, the histogram test is performed by capturing a block of data with no input signal, which you've already done. Instead of averaging the captured output data, however, make a histogram instead. A typical high-speed ADC might specify 1-LSB rms input noise, so you might see a Gaussian distribution with the offset ±3 codes. The input referred noise is calculated as the standard deviation of the captured data.

So, getting back to the original question, the wideband noise contributed by the ADC will cause the outputs to switch, even with no input signal. Good luck with the rest of your debug.



For More Information

Analog Dialogue:

"Rules of the Road" for High-Speed Differential ADC Drivers (pdf)
Wideband ADC Front-End Design: Amplifier Drive vs. Transformer Drive (Ask The Applications Engineer—36) (pdf)
ADC Input Noise: The Good, The Bad, and The Ugly. Is No Noise Good Noise? (pdf)
Transformer-Coupled Front-End for Wideband A/D Converters (pdf)
Pushing the State of the Art with Multichannel A/D Converters (pdf)
Which ADC Architecture Is Right for Your Application? (pdf)

RAQs:

Crosstalkin' Converters
Balancing Phase in High-Speed Converters
Bring on the Converter Noise!

Technical Articles:

Seven Steps to Successful Analog-to-Digital Signal Conversion (Noise Calculation for Proper Signal Conditioning) (pdf)
Nine Often Overlooked ADC Specifications (pdf)
High Speed Differential ADC Driver Design Considerations (pdf)

Technical Books:

Overview of DAC and ADC Architectures (pdf)
High Speed Sampling and High Speed ADCs (pdf)

Technical Books:

MT-006: ADC Noise Figure – An Often Misunderstood and Misinterpreted Specification (pdf)
MT-003: Understand SINAD, ENOB, SNR, THD, THD + N, and SFDR so You Don't Get Lost in the Noise Floor (pdf)

  • About The Author
  • David Buchanan
    Product Applications Engineer Manager, Analog Devices