DIRECT DIGITAL SYNTHESIS ICS DELIVER POWER AND SIZE SAVINGS

Direct Digital Synthesis ICs Deliver Power and Size Savings

Norwood, MA (04/25/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal processing applications, today introduced direct digital synthesis (DDS) ICs that offer 30 percent lower power consumption and a 60 percent reduction in footprint than competing devices while operating over the extended temperature range of -40º C to 125º C. The AD9838 DDS and AD9837 DDS ICs consume as little as 11 mW when operating from clock rates up to 16 MHz. The new devices are well suited for industrial and communications applications, including sensory excitation, impedance spectroscopy and battery-enabled diagnostic and communication equipment.

The AD9838 DDS and AD9837 DDS ICs settle in nanoseconds with granularity well below 100 mHz. Along with an on-chip, 10-bit, low-power DAC (digital-to-analog converter), the new products offer 28-bit fine-tuning granularity and high SFDR (spurious-free dynamic range) performance that enable them to more quickly and accurately generate a stable signal in the band of interest.

AD9838 DDS and AD9837 DDS ICs Feature Small Package Size

  • The small package size of the AD9838 DDS (4 mm × 4 mm) and AD9837 (3 mm × 3 mm) DDS ICs allows developers to reduce the footprint of their designs or increase sensor-node density to enable the development of feature-rich applications within the same form factor.
  • Low-power performance enables engineers to generate high-performance sine, square, and triangular outputs to meet the low-power consumption targets of battery-operated equipment or include advanced features within existing power budgets.
  • Integration of various communication and modulation features enables the devices to support single-tone, 2FSK, 2PSK, QPSK, sweep capability and amplitude modulation, simplifying the design of communication systems and reducing development risk and cost.
  • High spectral performance (greater than 68-dB wideband SFDR) enables product developers to keep pace with evolving needs in instrumentation and communication equipment.

Pricing, Availability and Complementary Components

Product Description Sample Availability Full-Volume Production Price Each
in 1,000 Quantities
Packaging
AD9838

Low-power DDS featuring differential current output with on-board comparator for clock generation

Now Now $2.10

20-lead
4 mm × 4 mm LFCSP

AD9837

Low-power DDS with voltage output

Now Now $1.65

10-lead
3 mm × 3 mm LFCSP

Complementary components for the AD9838 DDS and AD9837 DDS ICs include the AD9913 DDS, AD9707 TxDAC® DAC converter, AD5791 20-bit DAC and AD5543 16-bit multiplying DAC.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.

TxDAC is a registered trademark of Analog Devices, Inc.

Editor's Contact Information:

Linda Kincaid
781-937-1472

linda.kincaid@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close