CN0058

Sample-and-Hold Circuit Using the ADG1211 Switch
Manufactured by:

Circuit Function & Benefits

X+

This circuit is a sample-and-hold amplifier (SHA) function, which is basic to the data acquisition and analog-to-digital conversion process. In some programmable logic controller (PLC) output modules, a sample-and-hold in each channel stores the output samples from a single high performance DAC. The sample-and-holds are often implemented using analog switches or multiplexers and buffers. The circuit shown in Figure 1 provides a precise, fast sample-and-hold circuit capable of processing industrial-level signals of up to ±10 V.



Figure 1. High Precision Fast Sample-and-Hold Circuit (Simplified Schematic: Decoupling and All Connections Not Shown)


Switches and multiplexers are useful in data acquisition applications where instantaneous analog values must be captured. The input signal from the analog switch charges a hold capacitor that is connected to the input of an op amp. Ideally, the closed switch conveys nothing but the input signal to the capacitor. However, the switch also delivers a packet of charge when it switches, called charge injection. The ADG1211 quad SPST switch has excellent charge injection performance of only 1 pC compared to the next best solutions on the market, which have 10 pC to 20 pC of charge injection. The ADG1211 also has low capacitance and leakage current, making it an ideal choice for this circuit.

Circuit Description

X+

This is a precise, fast sample-and-hold circuit. During the sample mode, SW2 is closed, and the output, VOUT, follows the input signal, VIN. In the hold mode, SW2 is opened, and the signal is held by the hold capacitor, CH.


Due to switch and capacitor leakage current, the voltage on the hold capacitor decays (droops) with time. The ADG1211 minimizes this droop due to its low leakage specifications. The ADG1211 has 20 pA leakage typically at 25°C and 100 pA maximum. The droop rate is further minimized by the use of a polystyrene hold capacitor.

A second switch, SW1, which operates in parallel with SW2, is included in this circuit to reduce pedestal error. Since both switches are at the same potential, they have similar transients, which act as a common-mode signal to the op amp, thereby minimizing charge injection effects. Pedestal error is also reduced by the compensation network RC and CC. This compen-sation network also reduces the hold-time glitch, while optimizing the acquisition time.


The circuit in Figure 1 gives the following results: droop rate of 2 mV/ms, pedestal error of less than 0.5 mV, and acquisition time of 3 ms.

The circuit must be constructed on a multilayer PC board with a large area ground plane. Proper layout, grounding, and decoupling techniques must be used to achieve optimum performance (see Tutorial MT-031 and Tutorial MT-101).

Sample Products

X+

Samples

Product

Description

Available Product
Models to Sample

ADG1211 Low Capacitance, Low Charge Injection ±15 V/+12 V iCMOS Quad SPST Switches

ADG1211YCPZ-500RL7

ADG1211YRUZ

AD8672 Precision Low Noise, Low Input Bias Current Dual Op Amp

AD8672ARMZ

AD8672ARZ

AD8672TRZ-EP