CN0030

AD5390/AD5391/AD5392 Channel Monitor Function
Manufactured by:

Circuit Function & Benefits

X+

In a multichannel DAC system, the ability to monitor all outputs at a single point is a significant advantage for troubleshooting and diagnostic analysis. This circuit provides multichannel DAC output channel monitoring using a single-channel SAR ADC.


Figure 1. Efficient Channel Monitoring Circuit (Simplified Schematic)

Circuit Description

X+

This circuit utilizes the internal multiplexer on the AD5390/AD5391/AD5392 to route any of the DAC output channels to a single output pin (MON_OUT) for monitoring by the external ADC (AD7476). This approach utilizes much less circuitry than would be required if each channel were monitored individually.


The AD5390/AD5391 are complete, single-supply, 16-channel, 14-bit and 12-bit DACs, respectively. The AD5392 is a complete single-supply, 8-channel, 14-bit DAC. Devices are available both in 64-lead LFCSP and 52-lead LQFP packages. All channels have an on-chip output amplifier with rail-to-rail operation. The AD5390/AD5391/AD5392 contain a channel monitor function that consists of a multiplexer addressed via the serial interface, allowing any channel output to be routed to the monitor output (MON_OUT) pin for monitoring using an external ADC. The channel monitor function must be enabled in the control register before any channels are routed to MON_OUT. The AD5390/AD5391/AD5392 also include two uncommitted inputs (MON_IN1 and MON_IN2) to the internal multiplexer that allow the user the facility to monitor inputs from external sources such as references or power supplies. In Figure 1, the MON_IN1 pin on the AD5390 monitors the reference voltage from the AD780/ADR431.


The AD7476 ADC is a SAR ADC that offers 12-bit resolution, single 2.35 V to 5.25 V power supply, integrated reference, low power operation, small form factor, and serial interface, with throughput rates up to 1 MSPS in a 6-lead SOT-23 package. The reference for the part is taken internally from VDD, allowing the widest dynamic input range to the ADC. Thus, the analog input range for the part is 0 V to VDD. The conversion rate is determined by the SCLK, allowing throughput rates up to 1 MSPS.


The combination of the AD5390/AD5391/AD5392 and AD7476 provides a complete 8- or 16-channel analog output control solution with an efficient monitor function for system debug and fault and diagnostic analysis.


The AD5390/AD5391/AD5392 and the AD7476 must have ample supply bypassing of 10 μF in parallel with 0.1 μF on each supply pin, located as close to the packages as possible, ideally right up against the devices (this is not shown on the simplified diagram). The 10 μF capacitors are the tantalum bead type. The 0.1 μF capacitor must have low effective series resistance (ESR) and low effective series inductance (ESL), such as the common ceramic types, which provide a low impedance path to ground at high frequencies to handle transient currents due to internal logic switching.


The power supply traces should be as wide as possible to provide low impedance paths and reduce the effects of glitches on the power supply line. Fast switching signals, such as clocks, must be shielded with ground runs to avoid radiating noise to other parts of the board and must never be run near the analog signals. A ground line routed between the SDATA and SCLK lines helps reduce crosstalk between them (not required on a multilayer board, which has a separate ground plane; however, it is helpful to separate the lines). Avoid crossover of digital and analog signals. Traces on opposite sides of the board should run at right angles to each other. This reduces the effects of feedthrough on the board. A microstrip technique is recommended but not always possible with a double-sided board. In this technique, the component side of the board is dedicated to the ground plane, and signal traces are placed on the solder side. Best layout and performance is achieved with at least a 4-layer multilayer board, where there is a ground plane layer, a power supply layer, and two signal layers.

Common Variations

X+

Pin-compatible versions of the AD7476 are available for use in applications where lower resolution conversion is acceptable in the monitoring function. The AD7477 provides 10-bit resolution, and the AD7478 provides 8-bit resolution. The ADR431 reference can be substituted for the AD780.

Sample Products

X+

Samples

Product

Description

Available Product
Models to Sample

ADR431 Ultralow Noise XFET Voltage References with Current Sink and Source Capability

ADR431ARMZ

ADR431ARZ

ADR431TRZ-EP

AD7476 1MSPS, 12-Bit ADC in 6 Lead SOT-23

AD7476ARTZ-500RL7

AD7476SRTZ-EP-RL7

AD780 2.5 V/3.0 V High Precision Reference

Contact ADI

AD5391 16-Channel 3V/5V Serial Input Single-Supply 12-Bit Voltage-Output

AD5391BCPZ-3

AD5391BCPZ-5

AD5391BSTZ-3

AD5391BSTZ-5

AD5390 16-Channel 3 V/5 V Serial Input Single-Supply 14-Bit Voltage-Output

AD5390BCPZ-3

AD5390BCPZ-5

AD5390BSTZ-5

AD5392 8-Channel 3 V/5 V Serial Input Single-Supply 14-Bit Voltage-Output

AD5392BSTZ-5