Overview

Design Resources

Design & Integration Files

  • Schematic
  • Bill of Materials
  • Gerber Files
  • Allegro Files
  • Assembly Drawing
Download Design Files 3597 kB

Evaluation Hardware

Part Numbers with "Z" indicate RoHS Compliance. Boards checked are needed to evaluate this circuit

  • EVAL-CN0295-EB1Z ($85.00) Flexible, 4 mA-to-20 mA Pressure Sensor Transmitter with Voltage or Current Drive
Check Inventory & Purchase

Features & Benefits

  • 4-20mA transmitter
  • Voltage or current drive
  • Optimized for pressure sensors
  • Low Power

Circuit Function & Benefits

The circuit shown in Figure 1 is a flexible current transmitter that converts the differential voltage output from a pressure sensor to a 4 mA-to-20 mA current output.


The circuit is optimized for a wide variety of bridge-based voltage or current driven pressure sensors, utilizes only five active devices, and has a total unadjusted error of less than 1%. The power supply voltage can range from 7 V to 36 V depending on the component and sensor driver configuration.


The input of the circuit is protected for ESD and voltages beyond the supply rail, making it ideal for industrial applications.



Figure 1. Pressure Sensor Signal Conditioning Circuit with 4 mA-to-20 mA Output (Shown in Sensor Voltage Drive Mode) (Simplified Schematic: All Connections and Decoupling Not Shown)

Circuit Description

The design provides a complete solution for the 4 mA-to-20 mA transmitter for pressure sensor measurements. The circuit has three critical stages: the sensor excitation drive, the sensor output amplifier, and the voltage to current converter.


The total current required by the circuit (neglecting the bridge drive current and the output current) is 5.23 mA (maximum) as shown in Table 1.

Table 1. Maximum circuit currents at 25°C

Component
Current (mA)
ADR02
0.80
ADA4091-4
1.00
AD8226
0.43
R5, R6 at 6 V
0.60
R7, R8 at 5 V
0.40
R13 at 2 V
2.00
Total
5.23


Excitation: Voltage Drive Configuration

Depending on the pressure sensor selected, either a voltage or current drive is required. The circuit uses one-fourth of the ADA4091-4 (U2A) with different configurations chosen by switching S1 to support either option. Figure 2 shows the configuration for the voltage drive with S1 in the position closest to the identifying marking (see complete circuit layouts and schematics in the CN0295 design support package: http://www.analog.com/CN0295-DesignSupport). The voltage drive is normally configured for a bridge drive voltage of 6 V by the gain of the stage, 1 + R5/R6. Other drive voltages can be obtained by changing the resistor ratio appropriately:

CN0295_Image1


Note that the power supply voltage VCC should be at least 0.2 V greater than the bridge drive voltage to allow sufficient headroom for U2A, the ADA4091-4:

CN0295_Image2


CN0295_Image3


The ADA4091-4 op amp is chosen for the circuit because of its low current consumption (250 μA/amplifier), low offset voltage (250 μV), and rail-to-rail inputs and outputs.


The ADR02 is chosen for the 5 V reference because of its accuracy (A-Grade: 0.1%, B-Grade: 0.06%) and low quiescent current (0.8 mA).



Figure 2. Sensor Voltage Drive Configuration (Simplified Schematic: All Connections and Decoupling Not Shown)


Excitation: Current Drive Configuration

The circuit can be switched to the current drive configuration shown in Figure 3 by moving S1 to the position that is furthest away from the identifying marking.


In the current drive mode, the circuit is configured for R4 = 2.5 kΩ, and IDRIVE = 2 mA. Lower or higher values of IDRIVE can be obtained by using the following equation to select the value of R4:


CN0295_Image4


The resulting drive voltage VDRIVE is calculated from:


CN0295_Image5


A headroom of 0.2 V is required for the VCC supply, therefore:


CN0295_Image6


CN0295_Image7



Figure 3. Sensor Current Drive Configuration (Simplified Schematic: All Connections and Decoupling Not Shown)



Bridge Output Instrumentation Amplifier and Offset Circuit

The output of the bridge is filtered by a common-mode filter (4.02 kΩ, 1 nF) with a bandwidth of 39.6 kHz and a differential- mode filter (8.04 kΩ, 10 nF) with a bandwidth of 1.98 kHz.


The AD8226 is an ideal choice for the in-amp because of its low gain error (0.1%, B-grade), low offset (58 μV at G = 16, B-grade; 112 μV at G = 16, A-grade), excellent gain nonlinearity (75 ppm = 0.0075%), and rail-to-rail inputs and output.


The AD8226 instrumentation amplifier amplifies the 100 mV FS signal by a factor of 16 to 1.6 V using a gain setting resistor R3 = 3.28 kΩ. The relationship between the gain, G, and R3 is given by

CN0295_Image8


For G = 16, R3 = 3.2933 kΩ. The nearest standard 0.05% value of 3.28 kΩ is chosen for R3, yielding a gain of G = 16.06, which introduces an overall gain error of +0.4%.


For a 0 V bridge output, the output loop current should be 4 mA. This is achieved by simply applying a +0.4 V offset to the REF input of the AD8226 in amp as shown in Figure 1. The +0.4 V is derived from the ADR02 5 V reference using divider resistors R7/R8 and buffering the voltage with U2B.


The ADR02 5 V reference is used to set the drive voltage or current to the bridge and to set the 4 mA zero offset. It has an initial accuracy of 0.06% (B-grade) and 10 μV p-p voltage noise. In addition, it operates on supply voltages up to 36 V and consumes less than 1 mA, making it an ideal choice for low power applications.


Voltage to Current Conversion


The 0 V to 100 mV input to the AD8226 generates an output swing at VOUT of 0.4 V to 2.0 V. The buffer, U2C, applies this voltage across R13 that produces a corresponding current I13 of 0.4 mA to 2.0 mA. Transistor Q1 then mirrors the I13 current to R12, and the resulting voltage is applied to R15, thereby developing the final loop current of 4 mA to 20 mA. Transistor Q1 should have a high gain of at least 300 to minimize the linearity error due to its base current.


The output transistor Q2 is a 40 V P-channel MOSFET power transistor capable of dissipating 0.75 W at 25°C. The worst-case power dissipation in the circuit is for an output current of 20 mA into a loop load resistance of 0 Ω with a VCC supply of 36 V. Under these conditions the power dissipation of Q2 is 0.68 W. However, the power in Q2 can be significantly reduced by properly selecting VCC so that it is at least 3 V greater than the maximum loop load voltage. This ensures sufficient headroom due to the voltage dropped across the sense resistor R15.



Voltage Supply Requirement

In order for the circuit to operate properly, the supply voltage, VCC, must be greater than 7 V in order to provide sufficient headroom for the ADR02 voltage reference.


The minimum VCC supply voltage is also dependent on the configuration of the drive circuit for the bridge. In the voltage drive mode with VDRIVE = 6 V, the supply voltage VCC must be greater than 6.2 V in order to maintain sufficient headroom for U2A (see Figure 2).


In the current drive mode, the supply voltage VCC must be greater than 11.2 V in order to maintain sufficient headroom for U2A (see Figure 3).


The VCC supply voltage is limited to 36 V maximum.



Error Analysis for Active Components


The maximum and rss errors due to the active components in the system for A- and B-grade levels of the AD8226 and the ADR02 are shown in Tables 2 and 3. Note that the ADA4091-2 op amp is only available in one grade level. 


Table 2. Errors Due to Active Components (A-Grade)

Error Component
Error
Error Value
Error %FSR
AD8226-A
ADR02-A
ADA4091-4 (U2B)
ADA4091-4 (U2C)
ADA4091-4 (U2D)
AD8226-A 
Offset
Offset
Offset
Offset
Offset
Gain
112 µV
0.10%
250 µV
250 µV
250 µV
0.15%
0.11%
0.02%
0.02%
0.02%
0.02%
0.15%
RSS Offset
RSS Gain
RSS FS Error


0.12%
0.15%
0.27%
Max Offset
Max Gain
Max FS Error


0.19%
0.15%
0.34%


Table 3. Errors Due to Active Components (B-Grade)
Error Component
Error
Error Value
Error %FSR
AD8226-B
ADR02-B
ADA4091-4 (U2B)
ADA4091-4 (U2C)
ADA4091-4 (U2D)
AD8226-B
Offset
Offset
Offset
Offset
Offset
Gain
58 µV
0.06%
250 µV
250 µV
250 µV
0.10%
0.06%
0.01%
0.02%
0.02%
0.02%
0.10%
RSS Offset
RSS Gain
RSS FS Error


0.07%
0.10%
0.17%
Max Offset
Max Gain
Max FS Error


0.13%
0.10%
0.23%


Total Circuit Accuracy

A good approximation to the total error contributed by the resistor tolerances is to assume that each of the critical resistors contribute equally to the total error. The six critical resistors are R3, R7, R8, R12, R13, and R15. Worst-case tolerance build up of 0.1% resistors yields a total resistor error of 0.6% maximum. If rss errors are assumed, then the total rss error is 0.1√6 = 0.245%.


Adding the worst-case resistor tolerance error of 0.6% to the previous worst-case errors due to the active components (A- grade) yields:

  • Offset Error = 0.19% + 0.6% = 0.79%
  • Gain Error = 0.15% + 0.6% = 0.75%
  • Full Scale Error = 0.34% + 0.6% = 0.94%

These errors assume calculated resistor values are selected and that the only errors are due to their tolerances.

Although the circuit is capable of 1% or less total error, if better accuracy is required, add offset and gain adjustment capability to the circuit. Offset can be calibrated by adjusting R7 or R8 for 4 mA output with zero input, and full-scale can then be adjusted by varying R3 for a full-scale 100 mV input. The two adjustments are independent, provided the offset is calibrated first.


Actual error data from the circuit is shown in Figure 4 with VCC = 25 V. The total error in the output current (%FSR) is calculated by taking the difference between the ideal output current and the measured output current, dividing by the FSR (16 mA), and multiplying the result by 100.



Figure 4. Total Error in Output Current (%FSR) vs. Bridge Voltage for VCC = 25 V

0.07%
0.10%
0.17%
0.07%
0.10%
0.17%
0.13%
0.10%
0.23%

Common Variations

The circuit is proven to work with good stability and accuracy with component values shown. Other Analog Devices, Inc. voltage references, precision op-amps, and in-amps can be used in this configuration to develop 4 mA to 20 mA analog current output and for other various applications for this circuit.

The AD8426, a dual-channel, low cost and a wide supply range instrumentation amplifier can also be used for multiple input channel application.


The ADR4550, high precision, low power, low noise voltage references can be used to replace ADR02 for a low voltage supply applications.

Circuit Evaluation & Test

Equipment Required

  • EVAL-CN0295-EB1Z Evaluation Board
  • Agilent 36311A Precision DC Power Supply
  • Yokogawa 2000 Precision DC Power Supply
  • Agilent 3458A Precision Multimeter

The linearity error at the current output of the evaluation board was measured with a setup seen in Figure 5.

Figure 5. Block Diagram for the Test Setup


Test

Agilent E3631A and Yokogawa precision voltage supply were used to power up the board and simulate the sensor output. CH2 of Agilent E3631A was set at 25 V to serve as the power supply for the board and the other channel, CH1, was set at 2.5 V to generate common mode voltage. This channel was connected in series with the Yokogawa 2000 as shown in Figure 5. The Yokogawa generates the 0 to 100 mV differential input voltage at the in-amp input, which then simulates the sensor output.


The Agilent 3458A was used to measure the actual current output of the evaluation board, which is connected in series with J1.

Sample Products

Samples

Product

Description

Available Product
Models to Sample

ADR02 Ultracompact, Precision 5.0 V Voltage Reference

ADR02AKSZ-REEL7

ADR02ARZ

ADR02AUJZ-REEL7

ADR02WARZ-REEL7

AD8226 Wide Supply Range, Rail-to-Rail Output Instrumentation Amplifier

AD8226ARMZ

AD8226ARZ

ADA4091-4 Precision, Micropower, OVP, RRIO Quad Op Amp

ADA4091-4ACPZ-R7

ADA4091-4ARUZ

Buy functionality exists in desktop site
Evaluation Boards Pricing displayed is based on 1-piece.
Pricing displayed is based on 1-piece. The USA list pricing shown is for budgetary use only, shown in United States dollars (FOB USA per unit), and is subject to change. International prices may vary due to local duties, taxes, fees and exchange rates.