Overview

Features & Benefits

  • Low Jitter Clock Generator
  • Designed for High Speed ADCs
  • Optimized for High Precision, High Resolution and Low Noise

Circuit Function & Benefits

This circuit uses a direct digital synthesizer (DDS) with sub-Hertz tuning resolution as a low jitter sampling clock source for high performance ADCs. The AD9515 clock distribution IC provides PECL logic levels to the ADC. However, the AD9515 internal divider feature also allows the DDS to run at a higher frequency into the AD9515 front end, effectively increasing input slew rate. A higher slew rate into the AD9515 input squaring circuit can help reduce broadband jitter in the clock path.

Jitter on the ADC sampling clock produces degradation in the overall signal-to-noise ratio (SNR). The relationship is given by Equation 1.

cn0109_formula1 

where f is the full-scale analog input frequency, and tj is the rms jitter. "SNR" in Equation 1 is the SNR due solely to clock jitter and does not depend on the resolution of the ADC. 


The following data supports low jitter attainable from a DDS in clocking applications. Further details on Equation 1 and its use for evaluating the jitter on ADC sampling clocks can be found in Application Note AN-501.

Figure 1: DDS-Based ADC Sampling Clock Generator (Simplified Diagram)

Circuit Description

The circuit configuration in Figure 1 shows a DDS-based clock generator, consisting of a DDS followed by a reconstruction filter and an AD9515 clock distribution IC, used to provide the sampling clock for an analog-to-digital converter (ADC). The DDS sampling clock is derived from a Rohde and Schwarz SMA signal generator. The jitter measurement was made by using the clock derived from the DDS and the AD9515 as the sampling clock for the high performance AD6645 14-bit, 80 MSPS/105 MSPS ADC. The analog input signal for the ADC is a filtered 170.3 MHz sine wave derived from a low jitter Wenzel crystal oscillator (www.wenzel.com). Data was taken on two different DDSes: the AD9958 (500 MSPS) and the AD9858 (1 GSPS).

By evaluating the contribution of the ADC’s differential non-linearity and thermal noise and then applying the DDS-based clock and measuring the ADC SNR, the added jitter attributable to the DDS-based clock can be derived. For more details on the measurement setup and the jitter calculations, refer to Application Note AN-823. Also, Application Note AN-837 is instructive for designing DAC reconstruction filters with optimal stop-band performance.

Table 1 shows data for the AD9958 test results. The data confirms that better jitter performance is achieved as the frequency, or slew rate, of the DDS output frequency is increased and as the DDS output filter pass band is decreased. Table 2 shows the AD9858 with a 5% band-pass filter, a 225 MHz low-pass filter, and various levels of DDS output power. As expected, lower jitter is achieved as power is increased and bandwidth reduced. With a 5% band-pass filter, the majority of the spurs from the DAC are attenuated. The jitter in this case is much more dependent on noise coupling between the DAC output and the limiter input. This is proven by the strong correlation between jitter reduction and increased slew rate. Note that rms jitter values consistently less than 1 ps can be achieved using the AD9858 circuit.
  

Table 1. Jitter Response of AD9958 and AD9515 vs. fOUT, Power, Frequency, and Filter BW


Product  DDS Sample Rate (MHz)  DDS Output Frequency (MHz)  DDS Output Power (dBm)  DDS Reconstruction Filter (MHz)  AD9515 Divider Output Setting  AD9515 Output Frequency (MHz)  Jitter (rms) (ps) 
AD9958/AD9515
500
38.88
−3.6
200 LPF
1
38.88
4.1
AD9958/AD9515
500
38.88
−3.6
200 LPF
2
19.44
4.1
AD9958/AD9515
500
38.88
−4.7
47 LPF
1
38.88
2.4
AD9958/AD9515
500  38.88
−4.7
47 LPF
2
19.44
2.4
AD9958/AD9515
500
38.88  −3.3
5% BPF
1
38.88
1.5 
AD9958/AD9515  500
38.88
−3.3
5% BPF
2
19.44
1.5
AD9958/AD9515
500
77.76
−3.8
200 LPF
1
77.76
2.5
AD9958/AD9515
500
77.76
−3.8  200 LPF
2, 4  38.88, 19.44
2.5
AD9958/AD9515
500
77.76
−4.9
85 LPF
1
77.76
1.5
AD9958/AD9515
500
77.76
−4.9
85 LPF
2, 4
38.88, 19.44
1.5 
AD9958/AD9515
500
77.76
−3.8
5% BPF
1
77.76  1.1
AD9958/AD9515
500
77.76
−3.8
5% BPF
2, 4  38.88, 19.44
1.1
AD9958/AD9515  500
155.52
−5.5
200 LPF
2
77.76
1.5
AD9958/AD9515
500
155.52  −5.5  200 LPF
4, 8
38.88, 19.44
1.5
AD9958/AD9515
500
155.52  −5.6
5% BPF
2
77.76
0.68
AD9958/AD9515
500
155.52
−5.6
5% BPF
4, 8
38.88, 19.44
0.68

These circuits must be constructed on multilayer PC boards with large area ground planes using proper grounding, layout, and decoupling techniques (see MT-031 Tutorial, Grounding Data Converters and Solving the Mystery of AGND and DGND and MT-101 Tutorial, Decoupling Techniques) in order to achieve these performance levels. Consult the evaluation board documentation for the AD9958, AD9858, AD9515, and AD6645 for more guidance.


Table 2. Jitter Response of AD9858 and AD9515 vs. fOUT, Power, Frequency, and Filter BW


Product  DDS Sample Rate (MHz)  DDS Output Frequency (MHz)  DDS Output Power (dBm)
DDS Reconstruction Filter (MHz)  AD9515 Divider Output Setting  AD9515 Output Frequency (MHz)  Jitter (rms) (ps)
AD9858/AD9515
1000
155.52
+7.7
225 LPF
2
77.76
0.56
AD9858/AD9515
1000
155.52
+7.7
225 LPF
4,8
38.88, 19.44
0.56
AD9858/AD9515
1000
155.52
+7.7  5% BPF
2
77.76
0.33
AD9858/AD9515  1000  155.52
+7.7
5% BPF
4,8
38.88, 19.44
0.33
AD9858/AD9515
1000
155.52
+2.6
225 LPF
2
77.76
0.63
AD9858/AD9515
1000
155.52
+2.6
225 LPF
4,8
38.88, 19.44
0.63
AD9858/AD9515
1000
155.52
+1.1
5% BPF  2
77.76
0.42
AD9858/AD9515
1000
155.52
+1.1
5% BPF  4,8
38.88, 19.44
0.42
AD9858/AD9515
1000
155.52
−3.2
225 LPF
77.76
0.73
AD9858/AD9515
1000
155.52
−3.2
225 LPF
4,8
38.88, 19.44
0.73
AD9858/AD9515
1000
155.52
−4.6
5% BPF
2
77.76
0.64
AD9858/AD9515
1000
155.52
−4.6
5% BPF
4,8
38.88, 19.44
0.64


Common Variations

Analog Devices offers a variety of direct digital synthesizer, clock distribution chips, and clock buffers to build a DDS-based clock generator. Refer to www.analog.com/dds and www.analog.com/clock for more information.

Sample Products

Samples

Product

Description

Available Product
Models to Sample

AD9515 1.6 GHz Clock Distribution IC, Dividers, Delay Adjust, Two Outputs

Contact ADI

AD6645 14-Bit, 80 MSPS/105 MSPS A/D Converter

Contact ADI

AD9514 1.6 GHz Clock Distribution IC, Dividers, Delay Adjust, Three Outputs

Contact ADI

AD9912 1 GSPS Direct Digital Synthesizer with 14-Bit DAC

Contact ADI

AD9858 1 GSPS Direct Digital Synthesizer

Contact ADI

AD9512 1.2 GHz Clock Distribution IC, Two 1.6 GHz Inputs, Dividers, Delay Adjust, Five Outputs

Contact ADI

AD9910 1 GSPS, 14-Bit, 3.3 V CMOS Direct Digital Synthesizer

Contact ADI

AD9954 400 MSPS, 14-Bit, 1.8 V CMOS, Direct Digital Synthesizer

Contact ADI

AD9911 500 MSPS Direct Digital Synthesizer with 10-Bit DAC

Contact ADI

AD9913 Low Power 250 MSPS 10-Bit DAC 1.8 V CMOS Direct Digital Synthesizer

Contact ADI

AD9958

2-Channel, 500 MSPS DDS with 10-Bit DACs

Contact ADI

AD9513 800 MHz Clock Distribution IC, Dividers, Delay Adjust, Three Outputs

Contact ADI

AD9959 4 Channel 500 MSPS DDS with 10-bit DACs

Contact ADI

Buy functionality exists in desktop site