Norwood, MA (02/13/2013) - Analog Devices, Inc. (NASDAQ: ADI) today introduced a clock buffer and divider IC (integrated circuit) that combines high-speed, extremely low jitter (41 fs across the 12-kHz to 20-MHz band) and selectable division capability. The 1.65-GHz AD9508 clock buffer is designed for communications, instrumentation, defense and aerospace equipment that require ultra-high-speed data conversion with optimum SNR (signal-to-noise ratio) performance. The device has four dedicated output dividers with bus-programmable division (integers up to 1024) and phase delay, and automatic synchronization. The dividers also have pin-strapping capability for hardwired programming at system power-up. The AD9508 supports up to four differential, or eight single-ended outputs and three logic levels: LVDS (1.65 GHz), HSTL (1.65 GHz), and CMOS (250 MHz).
| Product | Availability | Temperature Range | Price each in 1,000 quantity | Packaging |
|---|---|---|---|---|
| AD9508 | NOW | -40°C to 85°C | $4.25 | 24-lead LFCSP |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
EngineerZone is a registered trademark of Analog Devices, Inc.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Jim Surber
336-605-4365
jim.surber@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved