Webcasts from Analog Devices


Webinar: Digital Potentiometers - Where and How to Use

VIEW THIS WEBCAST
(Registration required)
Digital Potentiometers (digiPOTs) provide a convenient way to adjust the ac or dc voltage or current output of sensors, power supplies, or other devices that require some type of calibration. This webcast will describe the function, use and advantages of using digital potentiometers in various applications. The webinar will also highlight the main parameters to be considered when designing a circuit using a digital potentiometer.
Presenter: David Rice and Joseph Creech
Application and Marketing Engineers
Analog Devices, Inc.

David Rice is an applications engineer in the Precision Converters group in ADI Limerick. David joined ADI in 2012 after graduating with a Masters degree in Embedded Systems Engineering from Cork Institute of Technology.

Joseph Creech earned his BEng from the University College Cork in 2005 and his MBA from the University of Limerick in 2013. Joseph has worked in ADI since 2005 in various product lines in applications and evaluation functions. Joseph is currently the marketing engineer for the digiPOT portfolio.

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close