content here.
content here.

Rarely Asked Questions...

A monthly column, "Rarely Asked Questions: Strange but true stories from the call logs of Analog Devices,"
is published monthly in EDN and Design News.

Single Supply Amplifiers–They Sound Simple ... are they?

Q. Running rail-to-rail op amps on a single supply sounds like a winning combination, but what drawbacks will I encounter when using amplifiers like this?

Single Supply Amplifiers

A.  Single-supply and rail-to-rail outputs are a great combination, but there are a few parameters that warrant a second look. Your question doesn’t specify whether you are talking about single-supply amplifiers (a particular class of amplifiers) or running a traditional op amp on single supply; we’ll discuss both cases.

By definition, a true "single-supply" op amp operates on one supply, and the input common-mode voltage range of the amplifier includes the negative supply rail. Note that even though the input of the amplifier can go to the negative rail and beyond it doesn't mean the output can. I'll say more about that when we talk about rail-to-rail outputs.

Any amplifier can be run on a single supply. Op amps don't have a ground pin and are equally happy when run on a bipolar supply as they are with a single supply. Additional bias circuitry is required when running an amplifier in this configuration, however. As a result, the amplifier's performance may suffer slightly in the following areas: lower bandwidth, degraded power supply rejection (PSR), and higher noise.

The term rail-to-rail output is a misnomer. While the amplifier output can get close to the supply rails, it never quite gets there. In bipolar amplifiers, the rail-to-rail output stage is typically a common emitter; therefore the closest the output can get to the rails is a saturated transistor drop Vcesat. The value of Vcesat is dependant on the amound of load current delivered by the amplifier. For low currents, the output can come to within tens of millivolts to the rail. For higher currents Vcesat can approach 0.5 V or more. Some new amplifiers now feature on-chip charge pumps to make up the Vcesat drop, allowing the output to truly swing all the way to the rail.

An amplifier output swinging close to the supply rail may appear fine when measured on an oscilloscope, but a network analyzer may reveal a different result. As the ouput swings close to the rails, the ouput transistors no longer operate in the linear region. As a result, distortion is introduced. Distortion can occur several hundreds of millivolts away from the rails. Therefore when possible, try to design in a little extra headroom from the rails; this will help improve the amplifier distortion performance.

Download this article (pdf, 119,519 bytes) back to top

John Ardizzoni is an Application Engineer at Analog Devices in the High Speed Amplifier Group. John joined Analog Devices in 2002, and has over 28 years experience in the electronics industry. John Ardizzoni


For more information:

Technical Articles:
Fast Rail-to-Rail Operational Amplifiers Ease Design Constraints in Low Voltage High Speed Systems (pdf, 234,127 bytes)

Design Assistants/Tools:
Multisim SPICE Program Download

Product Links:
AD8061: Low Cost, 300 MHz Rail-to-Rail Amplifier (Single)
AD8027: Low Distortion, High Speed Rail-to-Rail Input/Output Amplifier
AD8029: Low-Power High-Speed Rail-to-Rail Input/Output Op-Amp
AD8031: 2.7 V, 800 µA, 80 Mhz Rail-to-Rail I/O Single Amplifier

Analog Dialogue:
Avoiding Op-Amp Instability Problems In Single-Supply Applications
A Practical Guide to High-Speed Printed-Circuit-Board Layout

Press Releases:
Analog Devices High-Performance Amplifiers Deliver Sharper, More Life-Like Images In Hd Multimedia Applications

Online Seminars / Training/Tutorials:
Practical Analog Design Techniques Section 1: Single-Supply Amplifiers

Analog is everywhere

Useful Analog Devices Links:
Solutions Bulletin Library
Analog Devices Technical Bookstore
Sign up for Analog Devices eNewsletters

Analog Devices Homepage


back to top