CN0266: High Performance Digital MEMS Microphone Standard Digital Audio Interface to Blackfin DSP

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 06/2012 (pdf, 139 kB)
Benefits & Features
  • Connects directly to processor using simplified I2S interface
  • Up to 8 channels can be measured
  • MEMs microphone with flat wideband response
  • High performance microphone circuit
Products Used
    Applications: 
  • Communications
  • Consumer
  • Infotainment
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Design & Integration Files
(zip 3 kB)
  • Schematic
  • Bill of Materials
  • Layout Files
  • Assembly Drawing
Evaluation Hardware
Part numbers with "Z" indicate RoHS Compliance.
Boards checked are needed to evaluate this circuit.
  • EVAL-ADMP441Z ($200.00) High Performance Digital MEMS Microphone Standard Digital Audio Interface to Blackfin DSP
  • EVAL-SDP-CB1Z ($99.00) Eval Control Board
Check Inventory & Purchase
Connectivity Options
This circuit supports 3rd party connectivity.
Device Drivers
Software, such as C code and/or FPGA code, used to communicate with a component's digital interface.

CIRCUIT FUNCTION AND BENEFITS

The circuit shown in Figure 1 allows up to two digital MEMS microphones to be interfaced to a DSP on a single data line. The ADMP441 consists of a MEMS microphone element and an I2S output. This allows stereo microphones to be used in an audio system without the need for a codec between the microphones and the processor. Analog Devices, Inc., MEMS microphones have a high signal-to-noise ratio (SNR) and a flat wideband frequency response, making them an excellent choice for high performance, low power applications.

Up to two ADMP441 microphones can be input to a single data line on the ADSP-BF527 Blackfin® processor. The ADSP-BF527 can be set up with up to four serial data inputs; therefore, up to eight ADMP441s can connect to a single DSP.

Figure 1. MEMS Microphone Connection to Blackfin DSP (Simplified Schematic: All Connections Not Shown)

CIRCUIT DESCRIPTION

The ADMP441 microphones are connected to the SPORT data input pins of the ADSP-BF527. The only necessary passive components in this circuit are a single 0.1 μF bypass capacitor for each ADMP441 and a large pull-down resistor (100 kΩ) on the SD line to discharge it while the ADMP441 output drivers are tristated. Place the bypass capacitors as close to the ADMP441 VDD pin (Pin 7) as possible.

Supply the microphones' VDD from the same source as the 2.25 V to 3.3 V VDDEXT of the ADSP-BF527. Even though the ADMP441 can operate with VDD between 1.8 V and 3.3 V, VDDEXT on the ADSP-BF527 must be a minimum of 2.25 V.

There are three signals that must be connected between the ADMP441 and ADSP-BF527 for the I2S data stream: frame clock, bit clock, and data. The ADSP-BF527 is the system clock master and generates the two I2S clocks.

This circuit demonstrates the microphones connected to a single data input on the SPORT0 of the Blackfin. Each of the two SPORTs of the ADSP-BF527 has two sets of data receive pins that enable up to eight channels of I2S audio in. Table 1 shows the connections when using the serial SPORT0 of the ADSP-BF527.

equation

Set the L/R pin on the two ADMP441s to opposite levels—one pulled to VDD and the other to GND. When pulled to GND, the microphone outputs its data on the left channel of the I2S stream, and when pulled to VDD, it outputs its data on the right channel.

The ADMP441 is enabled by pulling the CHIPEN pin high. This pin can be tied either directly to the VDD of the microphone, which keeps it always enabled while it is powered, or it can be connected to a GPIO on the ADSP-BF527, allowing the Blackfin to enable and disable the microphone.

The ADMP441 has a sensitivity of −26 dBFS. In most applications, the microphone outputs require some gain added in the signal path of the Blackfin. If gain is added to the signal in the DSP, the output of the processor must still be limited to 0 dBFS.

ADSP-BF527 Register Settings
The SPORT register settings to set the ADSP-BF527 into I2S master mode follow. A more detailed description of these register settings can be found in the ADSP-BF52x Blackfin Processor Hardware Reference.

Configure SPORT_RCR1, the primary receive configuration register, with the following nondefault settings:

  • RCKFE: Drive internal frame sync on falling edge of RSCLK
  • RFSR: Require RFS for every data-word
  • IRFS: Internal RFS used
  • IRSCLK: Internal receive clock select

Configure SPORT_RCR2, the secondary receive configuration register, with the following nondefault settings:

  • RSFSE: Receive stereo frame sync enable
  • SLEN: 32-bit word length

Set SPORT_RCLKDIV, the SPORT receive serial clock divider register, to 17 (0x0011) and set SPORT_RFSDIV to 31 (0x001F). This sets the proper clock frequencies for a 48 kHz frame clock and 3.072 MHz bit clock with a 120 MHz Blackfin system clock (SCLK).

The registers settings described can be applied to either SPORT0 or SPORT1 on the ADSP-BF527, depending on which is being used.

COMMON VARIATIONS

DSPs
This circuit can also be set up with other parts from the Blackfin family instead of an ADSP-BF527. See the appropriate data sheets for details on the differences in number of SPORT channels and other variations. Consult the Blackfin family product page at: http://www.analog.com/blackfin.

Microphones
By removing one of the ADMP441 microphones, a mono microphone circuit using a single ADMP441 can be set up. The other connections remain the same in this mono configuration.

Additional ADMP441 microphones can be connected to the SPORT inputs of the ADSP-BF527 in the same way as the first stereo pair.

CIRCUIT EVALUATION AND TEST

The easiest way to evaluate a system with the ADMP441 MEMS microphone connected via I2S to the ADSP-BF527 Blackfin DSP is to use the EVAL-ADMP441Z evaluation board and the Blackfin SDP. These boards are designed to work together and include code to enable the digital audio connection. When connected to the USB port of a PC, the system is identified as a standard USB audio interface and enables streaming of stereo audio from the microphones to the PC.

Equipment Needed
The two evaluation kits needed include the following:

For correct operation of the SDP board, the PC must have the following minimum configuration:

  • Windows XP Service Pack 2, Windows Vista (32-bit), or Windows 7 (32-bit).
  • USB 2.0 port

A second EVAL-ADMP441Z-FLEX can be connected to the interface board to enable stereo audio capture.

Getting Started

The microphone FLEX PCBs connect to the interface board with ZIF headers, J1 and J2, and the EVAL-ADMP441Z connects to the SDP-B with 120-pin header, J3.

The documentation for the SDP-B controller board and EVAL-ADMP441Z describes the system setup and gives complete schematics of the boards. The only external connections required are the USB connection to the PC and system power to the ADMP441 evaluation board.

Complete documentation for the EVAL-ADMP441Z evaluation board can be found in the UG-362 user guide.

Complete documentation for the SDP-B controller board can be found in the SDP-B User Guide, UG-277.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
ADMP441 Omnidirectional Microphone with Bottom Port and I2S Digital Output ADMP441ACEZ-RL7
ADSP-BF527 Low Power Blackfin Processor with Advanced Peripherals

To obtain samples of this part, please contact ADI

content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close