CN0303: MEMS-Based Vibration Analyzer with Frequency Response Compensation

Engineered. Tested. Ready to Integrate.Learn More

OVERVIEW

Circuit Note PDF, 07/2013 (pdf, 275 kB)
Benefits & Features
  • High-g MEMS-based vibration analyzer
  • Flat response to 22kHz
  • 70g, 250g, and 500g range
Products Used
    Applications: 
  • Process Control & Industrial Automation
  • Automotive
  • Motor and Power Control
  • Electronic Test & Measurement
  • Avionics
  • Building Control & Automation
  • Inverters
  • Drives
  • Servos and Robotics
  • Power Supplies
  • UPS
Design Resources
Design & Integration Files
  • Schematic
  • Bill of Materials
  • Gerber Files
  • PADS Files
  • Assembly Drawing
Download Design Files (1053 kB)
Evaluation Hardware
Part numbers with "Z" indicate RoHS Compliance.
Boards checked are needed to evaluate this circuit.
  • EVAL-CFTL-6V-PWRZ ($17.00) Universal Power Supply
  • EVAL-CN0303-SDPZ ($70.00) MEMS-Based Vibration Analyzer with Frequency Response Compensation
  • EVAL-SDP-CB1Z ($99.00) Eval Control Board
Check Inventory & Purchase
Connectivity Options
This circuit supports 3rd party connectivity.

CIRCUIT FUNCTION AND BENEFITS

The circuit in Figure 1 offers a high linearity, low noise, wide-bandwidth vibration sensing solution. It is ideal for applications requiring a large dynamic range (±70 g, ±250 g or ±500 g) and a flat frequency response from dc to 22 kHz.

The circuit provides a low power solution suitable for bearing analysis, engine monitoring and shock detection.

The Analog Devices, Inc. proprietary fifth-generation iMEMs® process enables the ADXL001 accelerometer to provide dynamic range that extends from ±70 g to ±500 g in combination with 22 kHz of bandwidth.

The AD8606

The ADXL001 output voltage is converted into a digital word by the AD7476 low power, single channel 12-bit SAR ADC. is a precision, low noise, dual op amp used to create an analog bi-quad filter that flattens the output frequency response of the accelerometer

Figure 1. Single Axis Vibration Analysis System (Simplified Schematic: Decoupling and All Connections Not Shown)

CIRCUIT DESCRIPTION

Accelerometer Output Characteristics

The ADXL001 is specified and tested for 3.3 V and 5 V supplies. Although operational with a supply voltage anywhere between 3 V and 6 V, optimum overall performance is achieved at 5 V.

The output voltage sensitivity is ratiometric with respect to the supply voltage. For a 3.3 V supply, the nominal output sensitivity is 16 mV/g. For a 5 V supply, the sensitivity is 24.2 mV/g.

The zero-g output level is also ratiometric and is nominally equal to VDD/2.

The ADXL001 requires only one 0.1 μF decoupling capacitor as long as there is no noise present at the 1 MHz internal clock frequency. If necessary, larger bulk capacitors (1 μF to 10 μF) or ferrite beads can be included.

Accelerometer Physical Operation

The ADXL001uses silicon on insulator (SOI) MEMS technology and takes advantage of mechanically coupled but electrically isolated differential sensing cells. Figure 2 is a simplified view of one of the differential sensor cell blocks. Each sensor block includes several differential capacitor unit cells. Each cell is composed of fixed plates attached to the device layer, and movable plates attached to the sensor frame. Displacement of the sensor frame changes the differential capacitance. On-chip circuitry measures the capacitance change and converts it into an output voltage.

Figure 2. Simplified View of Sensor Under Acceleration

The sensor device is micro-machined in plane in the SOI device layer. Trench isolation is used to electrically isolate, but mechanically couple, the differential sensing elements. Single-crystal silicon springs suspend the structure over the handle wafer and provide resistance against acceleration forces.

The ADXL001 is an x-axis acceleration and vibration-sensing device. It produces a positive-going output voltage for vibration toward its Pin 8 marking as shown in Figure 3.

Figure 3. ADXL001 XOUT Voltage Increases with Acceleration in the Positive X-Axis Direction

Interfacing to the ADC

To digitize the acceleration information, the accelerometer output voltage range must fall inside the ADC input voltage range. The AD7476 input voltage range is 0 V to VDD (5 V). The ADXL001 output voltage range is 0.2 V to VS − 0.2 V (4.8 V). Based on this information, any acceleration sensed by the accelerometer will be digitized requiring no additional amplifiers or buffers.

Because the VDD power supply of the AD7476 serves as the ADC reference, an external reference is not required. In addition, the entire circuit is ratiometric with the supply because the same VDD supply also drives the ADXL001.

Frequency Response

The frequency response of the accelerometer is the most important characteristic in the system and is shown in Figure 4. As the frequency of the signal goes beyond approximately 2 kHz to 3 kHz, there is an increase in the gain of the accelerometer. At the resonant frequency of the beam (22 kHz), there is approximately 7 dB (×2.24) of peaking in the output voltage of the device. This peaking has significant ramifications for the output voltage of the accelerometer.

Figure 4. ADXL001 Frequency Response

Consider a 20 g acceleration at 10 kHz. The expected output voltage, assuming a zero-g output voltage of 2.5 V and a sensitivity of 24.2 mV/g is:


2.5 V + (0.0242 × 20) = 2.984 V

However, this voltage is increased by approximately 2 dB of peaking, causing the actual output voltage to be:

2 dB = 20 log10 (VOUT /2.984 V)
VOUT = 3.757 V

The difference between the expected output voltage and the actual output voltage is a significant source of error:

Error = 3.757 V – 2.984 V = 0.773 V

It is important to correct for this error to ensure accuracy, and an analog bi-quad filter was designed specifically for this purpose. The details of its implementation are discussed in the filter design section below.

Accelerometer Range Reduction

It is important to note, as the frequency response of the accelerometer begins to peak, the useable acceleration range of the device will decrease. Consider a 70 g acceleration at 20 kHz. The expected output voltage is:

2.5 V + (24.2mV/g × 70 g) = 4.194 V
Incorporating the ~7dB peaking effect:
7 dB = 20 log10 (VUT /4.194V)
VOUT = 9.389 V

Because the ADXL001 has a 5 volt supply rail, the output will limit at approximately +0.2 V and +4.8 V. The largest measureable g-force will therefore depend on the frequency of vibration.

Additional headroom of ±0.5 V must be allowed due to the variation in the zero-g offset voltage. The zero-g offset variation limits the maximum usable output voltage range to ±1.8 V, corresponding to approximately ±70 g for vibration frequencies less than about 2 kHz.

As the vibration frequency increases from about 2 kHz to 22 kHz, the maximum allowable g-force before output saturation is gradually reduced by 7 dB (×2.24) to ±31 g. As long as the maximum g-force is less than ±31 g, the filter provides a flat frequency response to 22 kHz without saturation and loss of information.

Filter Design

To compensate for the gain peak found in the accelerometer frequency response, an analog, bi-quad, notch filter was implemented. The quality factor (Q = 2.5) and resonant frequency of the beam (22 kHz) are both found in the specifications table of the ADXL001 datasheet.

By creating a notch filter with a peak of approximately −7 dB at 22 kHz, the frequency response of the accelerometer can be flattened, removing much of the difficulty in measuring vibration at higher frequencies. Figure 5 shows the frequency response for the filter, the accelerometer, and the entire signal chain. The data was taken using a sine wave input to the EVAL-CN0303-SDPZ board to simulate the accelerometer output.

Figure 5. ADXL001 Frequency Response, Filter Frequency Response and System Frequency Response

The notch filter was designed by modifying an example circuit found in “Passive and Active Network Analysis and Synthesis” by Aram Budak, October 1991 (ISBN-13: 978-0881336252. The transfer function for this compensator is the inverse of the previously derived transfer function. The Multisim™ Circuit Design Suite was used to simulate and verify the notch filter transfer function. The filter parameters were specified as Q = 2.5, center frequency = 22 kHz, notch depth = 7 dB.

Test Results

Two basic tests verify the performance of the system. First, a signal generator was used to drive a constant amplitude sine wave of varying frequency into the filter. Measuring the input and output voltages and plotting 20 log10(VOUT/VIN) provided the frequency response of the analog filter shown in Figure 5.

Second, the frequency response of the entire signal chain was verified to ensure the performance of the design. To more accurately verify the system frequency response, a signal generator was used to simulate the ADXL001 output.

For testing purposes, a 5 g acceleration was simulated and driven into the filter over a 50 kHz frequency range. If the ADXL001 were subject to a sinusoidal ±5 g acceleration in the sensitive axis, it would output a corresponding ac voltage:

±5 g × 0.0242V/g = ±0.121 V

This voltage is centered on the zero-g output, 2.5 V.

The signal generator drives this voltage into the filter. An oscilloscope was used to measure the peak output voltage of the filter. This voltage was converted back into g’s (divide g’s by the sensitivity) and compared to the original input acceleration. Plotting 20log10 (VOUT/VIN) provides the frequency response of the system.

It is important to adjust the signal generator output voltage based on the peaking found in the frequency response of the accelerometer. For a 10 kHz frequency, the output voltage of the signal generator must be increased by approximately 1.8 dB to accurately represent the output voltage of the accelerometer experiencing a 5 g acceleration.

The results of Figure 5 show the removal of the large peak found in the frequency response of the accelerometer. The −3 dB bandwidth is approximately 23 kHz. A small amount of ripple is seen in the passband immediately prior to the roll off caused by a slight misalignment in the peak of the accelerometer frequency response and the notch in the filter response.

A Wavetek Model 81 Pulse/Function Generator was used to generate a 2 kHz sine wave and connected directly to the filter input. Figure 6 shows a screen shot of the CN0303 Evaluation Software displaying conversion data from the AD7476 ADC and plotting the data in a graph. The sampling rate was 1 MSPS.

Figure 6. Screenshot of CN0303 Evaluation Software Digitizing a 2 kHz Sine Wave at a 1 MSPS Sampling Rate

PCB Layout Considerations

In any circuit where accuracy is crucial, it is important to consider the power supply and ground return layout on the board. The PCB should isolate the digital and analog sections as much as possible. The PCB for this system was constructed in a four-layer stack up with large area ground plane layers and power plane polygons. See the MT-031 Tutorial for more discussion on layout and grounding and the MT-101 Tutorial for information on decoupling techniques.

The EVAL-ADXL001-70Z board is connected to the EVAL-CN0303-SDPZ circuit board by a flexible ribbon cable. This allows the user to isolate the EVAL-CN0303-SDPZ from any vibrations that could cause potentially damaging mechanical stress to the circuit board as well as allowing the user to place the ADXL001 directly at the vibration source.

The power supply to the ADXL001 is decoupled with a 0.1μF capacitor to properly suppress noise and reduce ripple. The capacitor should be placed as close to the device possible.

Power supply lines should have as large a trace width as possible to provide low impedance paths and reduce glitch effects on the supply line. Clocks and other fast switching digital signals should be shielded from other parts of the board by digital ground.

A complete design support package for this circuit note can be found at www.analog.com/CN0303-DesignSupport.

Figure 7. Photo of EVAL-CN0303-SDPZ

COMMON VARIATIONS

To produce a more complete vibration sensing solution, a two axis ( ADXL2xx-family) or three axis ( ADXL3xx-family) accelerometer can be used in place of the ADXL001. By measuring acceleration in the second and third spatial dimensions, the user can write custom software allowing a more accurate and complete vibration sensing system.

CIRCUIT EVALUATION AND TEST

This circuit uses the EVAL-SDP-CB1Z System Demonstration Platform (SDP) evaluation board and the EVAL-CN0303-SDPZ circuit board. The two boards have 120-pin mating connectors, allowing for the quick setup and evaluation of the circuit’s performance.

This circuit also uses the EVAL-ADXL001-70Z evaluation board (included with the EVAL-CN0303-SDPZ board). The output connector (P1) of this PCB must be wired to the input connector (J6) of the EVAL-CN0303-SDPZ PCB using the ribbon cable supplied.

The EVAL-CN0303-SDPZ board contains the circuit to be evaluated, as described in this note. The EVAL-SDP-CB1Z evaluation board is used with the CN0303 Evaluation Software to capture the data from the EVAL-CN0303-SDPZ circuit board. The EVAL-ADXL001-70Z board contains the ADXL001 IC.

Equipment Needed

  • PC with a USB port and Windows® XP or Windows Vista® (32-bit), or Windows® 7 (32-bit)
  • EVAL-CN0303-SDPZ evaluation board
  • EVAL-ADXL001-70Z evaluation board and ribbon cable (included with EVAL-CN0303-SDPZ board)
  • EVAL-SDP-CB1Z evaluation board
  • CN0303 evaluation software
  • Power supply: +6.0 V or +6.0 V wall wart
  • Function generator (Wavetek 81 or equivalent) for generating simulated ADXL001 output if desired
Getting Started

Load the evaluation software by placing the CN0303 Evaluation Software disc in the CD drive of the PC. Using My Computer, locate the drive that contains the evaluation software disc and open the Readme file. Follow the instructions contained in the Readme file for installing and using the evaluation software.

Functional Block Diagram

A functional block diagram of the test setup is shown in Figure 8. The signal generator is used to simulate the ADXL001 output. The EVAL-ADXL001-70Z board can be connected to EVAL-CN0303-SDPZ board for actual vibration measurements by using the ribbon cable to connect the 5-pin header (P1) of the EVAL-ADXL001-70Z to the 5-pin header (J6) of the EVAL-CN0303-SDPZ.

Figure 8. Test Setup Functional Block Diagram

Setup

Connect the 120-pin connector (J1) on the EVAL-CN0303- SDPZ circuit board to the connector on the EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.

Connect the 5-pin header (P1) of the EVAL-ADXL001-70Z evaluation board to the 5-pin header (J6) of the EVAL-CN0303-SDPZ circuit board using the ribbon cable.

Connect a +6.0 V power supply to connector J5 of the EVAL-CN0303-SDPZ board. Connect the USB cable supplied with the SDP board to the USB port on the PC. Do not connect the USBcable to the mini USB connector on the SDP board at this time.

Test

Launch the Evaluation software, and connect the USB cable from the PC to the USB mini-connector on the SDP board.

After USB communications are established, the SDP board can now be used to send, receive, and capture serial data from the EVAL-CN0303-SDPZ board.

Information regarding the SDP board can be found in the SDP User Guide.

Information and details regarding test setup and calibration, and how to use the evaluation software for data capture can be found in the software Readme file found at: www.analog.com/CN0303-UserGuide.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
AD7476 1MSPS, 12-Bit ADC in 6 Lead SOT-23 AD7476ARTZ-500RL7 AD7476ARTZ-REEL7
AD8606 Precision, Low Noise, RRIO, CMOS Op Amp (Dual) AD8606ACBZ-REEL7 AD8606ARZ
ADXL001 High Performance Wide Bandwidth iMEMS® Accelerometer

To obtain samples of this part, please contact ADI

Evaluation Hardware
Boards checked are needed to evaluate this circuit.
Model Description Price RoHS Check Inventory/
Purchase/Sample
EVAL-CFTL-6V-PWRZ Universal Power Supply $17.00 Yes
EVAL-CN0303-SDPZ MEMS-Based Vibration Analyzer with Frequency Response Compensation $70.00 Yes
EVAL-SDP-CB1Z Eval Control Board $99.00 Yes
Pricing displayed is based on 1-piece. The USA list pricing shown is for budgetary use only, shown in United States dollars (FOB USA per unit), and is subject to change. International prices may vary due to local duties, taxes, fees and exchange rates.
沪ICP备09046653号
Review this Circuit X
content here.
content here.

Review this Circuit

Close