The circuit, shown in Figure 1, uses the ultralow power AD7982 18-bit, 1 MSPS ADC driven by the ADA4940-1, a low power fully differential amplifier. The ADR395, low noise precision 5.0V voltage reference is used to supply the 5 V needed for the ADC. All the ICs shown in Figure 1 are available in small packages, either 3 mm × 3 mm LFCSP, or 3 mm × 5 mm MSOP, which helps reduce board cost and space.
Power dissipation of the ADA4940-1 in the circuit is less than 9 mW. The 18-bit, 1 MSPS AD7982 ADC consumes only 7 mW @ 1 MSPS, which is much lower than competitive ADCs available in the market. This power also scales with the throughput. The ADR395 consumes only 0.7mW, making the total power dissipated by the system less than 17 mW.
|
|
Figure 1. High Performance 18-Bit Differential ADC Driver (Simplified Schematic: All Connections and Decoupling Not Shown)
|
Modern high resolution SAR ADCs, such as the AD7982 18-bit, 1 MSPS PulSAR® ADC, require a differential driver for optimum performance. In such applications, the ADC driver takes either a differential or single-ended signal and performs the level shifting required to drive the input of the ADC at the right level.
Figure 1 shows the ADA4940-1 differential amplifier level shifting and driving the 18-bit AD7982 differential input successive approximation PulSAR ADC. Using four resistors, the ADA4940-1 can either buffer the signal with a gain = 1 or amplify the signal for more dynamic range. The ac and dc performances are compatible with those of the 18-bit, 1 MSPS AD7982 PulSAR® ADC and other 16- and 18-bit members of the family, which have sampling rates up to 2 MSPS. This circuit can also accept a single-ended input signal to generate the same fully differential output signal.
The AD7982 operates on a single VDD supply of 2.5 V. It contains a low power, high speed, 18-bit sampling ADC and a versatile serial interface port. The reference voltage (REF) is applied externally from the ADR395 precision low dropout (0.3 V) band gap reference, and can be set independently of the supply voltage. The ADA4940-1 is dc coupled on the input and the output and performs a differential or single-ended-todifferential conversion if needed. It also buffers the driving signal. A single-pole 1.8 MHz R-C (33 Ω, 2.7 nF) noise filter is placed between the op amp output and the ADC input. The filter also provides some isolation between the op amp output and the switching spikes at the ADC input due to the internal sample-and-hold function.
The ADA4940-1 is driven with a 7 V supply (+6 V and –1 V) in order to provide sufficient headroom on the outputs, which must swing from 0 V to +5 V for a full-scale input to the ADC.
The gain is set by the ratio of the feedback resistor (R2 = R4) to the gain resistor (R1 = R3). In addition, the circuit can be used to convert either single-ended or differential inputs to a differential output. If needed, a termination resistor in parallel with the input can be used. Whether the input is a single-ended input or differential input, the input impedance of the amplifier can be calculated as show in the MT-076 Tutorial and in the DiffAmpCalc™ Differential Amplifier Calculator (www.analog.com/diffampcalc).
If R1 = R2 = R3 = R4 = 1 kΩ, the single-ended input impedance is approximately 1.33 kΩ. An external 52.3 Ω termination resistor provides a 50 Ω termination for the source. An additional 25.5 Ω (1025.5 Ω total) at the inverting input balances the parallel impedance of the 50 Ω source and the termination resistor driving the noninverting input (52.3 Ω || 50 Ω = 25.5 Ω). However, if a differential source input is used, the differential input impedance is 2 kΩ. In this case, two 52.3 Ω termination resistors are used to terminate each input if needed.
|
|
Figure 2. FFT Plot (32,000 Point) for 20 kHz Signal, 0.5 dB Below Full Scale, with Sampling Frequency of 1 MSPS
|
For the tests on this circuit, the signal generator provided a 10 V p-p differential output. The VOCM input is bypassed for noise reduction and set externally with 1% resistors to maximize the output dynamic range on the 5 V reference. With an output common-mode voltage of 2.5 V, each ADA4940-1 output swings between 0 V and 5 V, opposite in phase, providing a gain of 1 and a 10 V p-p differential signal to the ADC input. The FFT performance is shown in Figure 2 and is summarized as follows:
The INL and DNL performance are shown in Figure 3.
|
|
Figure 3. INL and DNL Plot for 20 kHz Signal, with Sampling Frequency of 1 MSPS
|
The circuit is proven to work with good stability and accuracy with component values shown. Other analog-to-digital converters can be used in place of the AD7982 to achieve the maximum desired performance. The ADA4940-1/ ADA4940-2 is optimum for driving 16-bit and 18-bit ADCs with minimal degradation in performance. Faster sampling 18-bit ADCs include the AD7984 (1.33 MSPS) and AD7986 (2 MSPS). Differential 16-bit ADCs include the AD7688 (500 kSPS) and the AD7693 (500 kSPS).
The ADA4940-1/ADA4940-2 rail-to-rail outputs can be driven to within 0.5 V of each power rail without significant ac performance degradation. Other differential ADC drivers such as the AD8137 and ADA4941-1 can also be used to replace the ADA4940-1 for other applications when speed, input impedance, or other factors dictate.
This circuit was tested using a modified EVAL-AD7982SDZ PulSAR AD7982 evaluation board connected to the converter evaluation and development board (EVAL-CED1Z).
The AD7982 evaluation board was modified to accept the ADA4940-1 differential ADC driver and the ADR395 reference.The EVAL-AD7982SDZ is a customer evaluation board intended to ease standalone testing of performance and functionality for the 18-bit AD7982 PulSAR ADC.
The EVAL-CED1Z board is a platform intended for use in evaluation, demonstration, and development of systems using Analog Devices precision converters. It provides the necessary communications between the converter and the PC, programming or controlling the device, transmitting or receiving data over a USB link as shown in Figure 4 and Figure 5.
|
|
Figure 4. PulSAR ADC Evaluation Platform
|
|
|
Figure 5. Test Setup Functional Block Diagram
|
Equipment Needed
In addition to the two evaluation boards, the external power
supplies of +6 V and –1 V were required for the ADA4940-1.
A "wall wart" supplied the +7.5 V dc voltage for the
EVAL-CED1Z. Other appropriate voltages were supplied to
the AD7982 evaluation board from the EVAL-CED1Z.
A low distortion signal source, the Audio Precision® SYS-2702, was used to achieve the required performance. A PC with Windows® XP or Windows 7 equipped with an USB port was used to run the PulSAR evaluation software.
Getting Started
The software was installed as described at www.analog.com/EVAL-CED1Z, and www.analog.com/AD7982_adc_EVAL-CED1Z.
The modified AD7982 evaluation board was connected to the EVAL-CED1Z. The +7.5 V wall wart was connected to the EVAL-CED1Z. The external power supplies of +6 V and −1 V were connected to the AD7982 evaluation board.
Setup and Test
An Audio Precision SYS-2702 source was used to provide the
input signal to the AD7982 evaluation board. The PulSAR
evaluation software, which is LabVIEW® based, was used to
control the Audio Precision input signals and also to monitor
the ADC inputs and output.