CN0207: High Performance Analog MEMS Microphone's Simple Interface to SigmaDSP Audio Codec

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 05/2011 (pdf, 126 kB)
Benefits & Features
  • MEMs microphone with flat wideband response
  • Interface connects directly with audio codec
  • Audio codec with DSP core which enhances post-processing
  • Low power, analog output, high performance microphone
    Applications: 
  • Consumer
  • Infotainment
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Design & Integration Files
(zip 2 kB)
  • Schematic
  • Bill of Materials
  • Assembly Drawing
Evaluation Hardware
Part numbers with "Z" indicate RoHS Compliance.
Boards checked are needed to evaluate this circuit.
  • EVAL-ADAU1761Z ($195.00) SigmaDSP Stereo, Low Power, 96 kHz, 24-Bit Audio Codec with Integrated PLL
  • EVAL-ADMP404Z-FLEX ($80.00) Omnidirectional Microphone with Bottom Port and Analog Output
Check Inventory & Purchase
Connectivity Options
This circuit supports 3rd party connectivity.
Device Drivers
Software, such as C code and/or FPGA code, used to communicate with a component's digital interface.

CIRCUIT FUNCTION AND BENEFITS

The circuit shown in Figure 1 allows up to two analog MEMS microphones to be interfaced to an audio codec. The ADMP404 consists of a MEMS microphone element and an output amplifier. Analog Devices, Inc., MEMS microphones have a high signal-to-noise ratio (SNR) and a flat wideband frequency response, making them an excellent choice for high-performance, low-power applications.

Up to two ADMP404 analog MEMS microphones can be input to an ADAU1761 low-power codec’s two ADCs.

Figure 1. Analog MEMS Microphone Connection to the Audio Codec (Simplified Schematic: Power Supply Decoupling and All Connections Not Shown)

CIRCUIT DESCRIPTION

The ADMP404 analog MEMS microphones are connected to the ADAU1761 LINN and RINN input pins. These pins are connected to the inverting inputs of the internal PGAs. The only necessary passive components in this circuit are a single 0.1 μF bypass capacitor for each ADMP404 and a 2.2 μF capacitor in series with each MEMS microphone output. The bypass capacitors should be placed as close to the ADMP404 VDD pin (Pin 3) as possible. The ADAU1761 LINP and RINP should be connected directly to the codec CM pin.

The ADMP404 power supply is provided from the ADAU1761 MICBIAS pin. MICBIAS can be set to either 0.9 × AVDD or 0.65 × AVDD, where allowable values of AVDD for the ADAU1761 are between 1.8 V and 3.3 V. The ADMP404 VDD supply should be between 1.5 V and 3.6 V.

The ADMP404 has a sensitivity of −38 dBV. In most applica-tions, the MEMS microphone outputs must have some additional gain, which is provided by the ADAU1761 internal PGAs. The input PGAs can be set for up to 35.25 dB of gain in 0.75 dB steps, with an additional fixed 20 dB boost available following the PGAs.

The PGA input and the ac-coupling capacitor between the MEMS microphone and codec form a high-pass filter. The −3 dB corner frequency of this filter is 1/(2πRC), where C is the capacitor size, and R is the codec’s input impedance for a given PGA gain setting. For a +20 dB gain setting (9.1 kΩ input impedance) and a 2.2 μF capacitor, the high-pass filter’s corner is 8 Hz. Increasing the PGA gain settings raises the filter corner frequency, whereas increasing the capacitor size lowers the corner frequency. See the ADAU1761 data sheet for details on the input impedance at different settings.

Register Settings
The following register bit fields must be set in the ADAU1761 to enable its PGAs and ADCs for microphone input on the left channel. Setting 1 to Setting 4 should be repeated for the register bit fields controlling the right channel if two MEMS microphones are used. These settings are:

  1. MX1EN in Register R4 to 0b1— enables the left channel input mixer.

  2. LDBOOST[1:0] in Register R5 to 0b01 for 0 dB additional boost and to 0b10 for 20 dB additional boost.

  3. LDVOL[5:0] in Register R8—sets the PGA input gain between −12 dB and 35.35 dB.

  4. LDEN in Register R8 to 0b1—enables the left differential input path.

  5. MBI in Register R10 to 0b0 for 0.90 × AVDD or to 0b1 for 0.65 × AVDD—sets the voltage level of the MICBIAS output.

  6. MBIEN in Register R10 to 0b1—enables the MICBIAS output.

  7. LDMUTE in Register R8 to 0b1—unmutes the left differential input channel. To avoid pops and clicks, this should be the last bit set.

A screen shot of the SigmaStudio™ register controls for the analog input is shown in Figure 2.

Figure 2. SigmaStudio PGA Input Configuration for the MEMS ADMP404 Microphone Input to the ADAU1761

In its default performance setting (MPERF = 0), the MICBIAS output sources up to approximately 2 mA of current to supply the microphone VDD supply. The ADMP404 draws a maximum of 250 μA; therefore, this bit does not need to be set to high performance (MPERF = 1), even to supply power to two microphones. The codec’s high-performance bias mode is only needed when biasing electret microphones, not for providing supply to MEMS microphones.

A complete design support documentation package for this circuit note can be found at http://www.analog.com/CN0207-DesignSupport.

COMMON VAIRATIONS

This circuit can also be set up with an ADAU1361 instead of an ADAU1761. The primary difference between these two codecs is that the ADAU1761 has a SigmaDSP® processor core and the ADAU1361 does not. The ADAU1781 SigmaDSP codec can also be used.

A mono microphone circuit using a single ADMP404 can be set up by simply removing one of the ADMP404 MEMS microphones and its associated capacitors. The other connections remain the same in this mono configuration.

The ADMP404 can also be replaced with an ADMP401, ADMP405, or ADMP504, which are also analog MEMS microphones. The ADMP401 has a −42 dBV sensitivity, whereas the ADMP404 has a −38 dBV sensitivity. The ADMP405 is identical to the ADMP404 except that the ADMP405 has a low frequency cutoff at 200 Hz vs. the ADMP404’s 100 Hz cutoff. This higher frequency cutoff makes the ADMP405 attractive for reducing low frequency wind noise. The ADMP504 has the same −38 dBV sensitivity as the ADMP404, but its noise floor is 3 dB lower. The ADMP504 and ADMP404 are pin and footprint-compatible.

CIRCUIT EVALUATION AND TEST

Evaluation boards for the ADMP404 and ADAU1761 are available and can easily be connected as described below.

Equipment Needed

The SigmaStudio GUI software requires a PC with the following: Windows® 7, Windows Vista, or Windows XP Professional or Home Edition with SP2, 128 MB of RAM (256 MB recom-mended), 50 MB of available hard disk space, 1024 × 768 screen resolution, and USB 1.1/2.0 data port.

In addition, the ADAU1761 Evaluation Board (EVAL-ADAU1761Z) and the ADMP404 Evaluation Board (EVAL-ADMP404Z-FLEX) are required.

Getting Started
The EVAL-ADMP404Z-FLEX has three output wires: VDD, GND, and OUTPUT. The VDD wire should be connected to J15 or J18 on the EVAL-ADAU1761Z board to supply power from the ADAU1761 MICBIAS pin. The output wire of the ADMP404 board can be connected to the tip of a mono 3.5 mm audio plug, with ground connected to the ring. This plug connects to the ADAU1761 evaluation board’s two analog input jacks: J20 and J22. The ADAU1761 evaluation board has 10 μF ac-coupling capacitors rather than the 2.2 μF capacitors shown in Figure 1.

From this point, follow the documentation for the EVAL-ADAU1761Z regarding software installation, setup, and operation of the system.

The SigmaStudio software is used to program and tune the registers and SigmaDSP core in the ADAU1761. SigmaStudio can be downloaded from http://www.analog.com/sigmastudio.

Functional Block Diagram
The documentation for the ADAU1761 evaluation board (EVAL-ADAU1761Z) describes the system setup and gives a complete schematic of the board. The only external connections required are the USB connection to the PC and to the audio outputs of the ADAU1761 evaluation board.

Setup and Test
See the EVAL-ADAU1761Z board documentation for addi-tional details regarding circuit description, jumper settings, setup, and testing.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
ADAU1761 SigmaDSP® Stereo, Low Power, 96 kHz, 24-Bit Audio Codec with Integrated PLL ADAU1761BCPZ
ADMP401 Omnidirectional Microphone with Bottom Port and Analog Output ADMP401ACEZ-RL7
ADMP404 Omnidirectional Microphone with Bottom Port and Analog Output ADMP404ACEZ-RL7
ADMP405 Omnidirectional Microphone with Bottom Port and Analog Output ADMP405ACEZ-RL7
ADMP504 UltraLow Noise Microphone with Bottom Port and Analog Output ADMP504ACEZ-RL7
content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close