CN0101: Reconstruction Video Filter Using the ADA4430-1 Amplifier After the ADV7393 Video Encoder

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 11/2010 (pdf, 112 kB)
Benefits & Features
  • Reconstruction Video Filter used after Encoder
  • Optimized for High Resolution and High Speed
  • Designed for Automotive Applications
    Applications: 
  • Asset Tracking
  • Consumer
  • Infotainment
  • Video Surveillance
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Connectivity Options
This circuit supports 3rd party connectivity.

CIRCUIT FUNCTION AND BENEFITS

This circuit illustrates a digital-to-analog video converter paired with a low cost, low power, fully integrated reconstruction video filter. Although many video encoders (video DACs) such as the ADV7393 can drive a video load directly, it is often very beneficial to use a video driver at the output of a video encoder for power savings, line driving, and additional circuit protection. The video driver is typically configured as an active filter, also known as a reconstruction or anti-imaging filter. The purpose of the reconstruction filter is twofold: it blocks the higher frequency components (above the Nyquist frequency) that were introduced into the video signal as part of the digitization process and provides gain to drive the external 75 Ω cable to the video display. For ac-coupled output applications, the ADA4430-1 has an integrated SAG correction network. Signal amplitude gain (SAG) correction is used to provide low frequency compensation for the high-pass filter formed by the 150 Ω video load of a back-terminated cable and the output coupling capacitor. SAG correction reduces the size of the traditionally large ac coupling capacitor (330 μF), replacing it with much smaller 47 μF and 22 μF capacitors.

The ADA4430-1 and the ADV7393 are both recommended for automotive application, which makes both products ideal for infotainment and vision-based safety systems applications.

Figure 1: Low Cost, Fully Integrated Reconstruction Filter using the ADA4430-1(Simplified Schematic)

CIRCUIT DESCRIPTION

The ADV7393 is a low power, fully integrated digital video encoder that converts digital 16-bit component video data, for example from a CMOS rearview camera, into a standard analog baseband video signal compatible with worldwide standards. The three 2.6 V/3.46 V 10-bit video DACs provide support for composite (CVBS), S-video (YC), or component (YPrPb/RGB) analog outputs in either standard definition (SD) or high definition (HD) video formats. The circuit in Figure 1 is configured for low output drive operation, which reduces the output current by 85% in all three DACs (RSET = 4.12 kΩ, RL = 300 Ω). To further save power, the internal PLL is disabled, and the encoder is operating in a 2× oversampling mode. The 16-bit video input port is configured to support SD video.

The ADA4430-1 is a single sixth-order, low-pass video filter with a 9 MHz −3 dB cutoff and 50 dB of out-of-band rejection at 27 MHz. The ADA4430-1 is a low power, low cost, rail-to-rail output amplifier that has an operating supply range of +2.5 V to +6 V and is ideal for SD video application. Combined with the ADV7393 single chip video encoder, the ADA4430-1 enables the most power efficient video output solution for automotive applications. In Figure 1, the ADA4430-1 is configured as a reconstruction video filter with ac-coupled output with SAG correction. The compensation network includes C1, C2, and the internal resistor network integrated into the ADA4430-1. Traditional ac-coupling uses a large, expensive coupling capacitor, making it costly and wastes valuable PCB space. SAG correction allows two small, low cost capacitors to replace the one large ac-coupling capacitor and still maintain the same field tilt. Field tilt is a measure of the voltage droop (tilt) that occurs on the ac-coupling capacitor when a constant luma signal is applied. This droop is caused by the small discharge current created by the 75 Ω load resistor. The SAG correction capacitor values were chosen so as to achieve the equivalent field tilt of a 220 μF ac-coupling capacitor.

When using the SAG correction circuit, the gain from the input to the immediate output of the ADA4430-1 is 2.5 (≈8 dB) at extremely low frequencies, where the outer feedback loop formed by the 22 μF capacitor effectively opens (see Figure 2) and exhibits a second-order peak of approximately 11 dB at approximately 5 Hz. This gain is approximately 7.5 dB at 30 Hz. The extra gain must be accounted for when considering low frequency input and output signal swings to keep them within their specified limits. The gain from the ADA4430-1 input to the load side of the 47 μF capacitor does not exhibit this behavior; instead, it appears more like a single-pole high-pass response.

Figure 2 illustrates the SAG frequency response immediately at the ADA4430-1 output and at the load side of the 47 μF capacitor.

Figure 2: SAG Correction Frequency Response at ADA4430-1 Output and at the Load Side of the 47 μF Capacitor

Buffering is a function that is often overlooked, but is very important. For example, many automotive customers will use low cost amplifiers to protect more expensive and complex devices, such as video decoders and encoders. Amplifiers with ac-coupled outputs as shown in Figure 1 help protect such devices from overvoltage and ESD damage.

COMMON VARIATIONS

There are a few options for ac-coupled output configuration. SAG correction, as shown in Figure 1, uses 22 μF and 47 μF capacitors. The traditional ac-coupled output uses a single 220 μF capacitor; in this configuration, the SAG pin is connected directly to the output pin before the output capacitor. For dc-coupled configurations, the SAG pin is also connected directly to the output pin. In both dc-coupled and traditional ac-coupled configurations, connecting the SAG pin directly to the output pin results in a gain of +2 buffer at all video frequencies.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
ADA4430-1 Ultralow Power Video Filter with Power-Down ADA4430-1YKSZ-R7
ADV7390 Low Power, Chip Scale 10-Bit SD/HD Video Encoder

To obtain samples of this part, please contact ADI

ADV7391 Low Power, Chip Scale 10-Bit SD/HD Video Encoder ADV7391BCPZ ADV7391BCBZ-A-RL ADV7391WBCPZ
ADV7392 Low Power, Chip Scale 10-Bit SD/HD Video Encoder

To obtain samples of this part, please contact ADI

ADV7393 Low Power, Chip Scale 10-Bit SD/HD Video Encoder ADV7393BCPZ
content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close