CN0041: DC-Coupled, Single-Ended-to-Differential Conversion Using the AD8138 Low Distortion Differential ADC Driver and the AD7356 5 MSPS, 12-Bit SAR ADC

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 09/2010 (pdf, 98 kB)
Benefits & Features
  • DC coupled
  • Single ended to differential conversion
  • Optimized ADC driver for high performance
  • Speeds up to 5 MSPS
Products Used
    Applications: 
  • Electronic Test & Measurement
  • Instrumentation
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Connectivity Options
This circuit supports 3rd party connectivity.

CIRCUIT FUNCTION AND BENEFITS

This circuit provides a dc-coupled, single-ended-to-differential conversion of a bipolar input signal to the AD7356 5 MSPS, 12-bit successive approximation register (SAR) analog-to-digital converter (ADC). This circuit is designed to ensure maximum performance of the AD7356 by providing adequate settling time and low impedance.

CIRCUIT DESCRIPTION

Differential operation requires VINx+ and VINx− of the ADC to be driven simultaneously with two equal signals that are 180° out of phase and are centered around the proper common-mode voltage. Because not all applications have a signal preconditioned for differential operation, there is often a need to perform a single-ended-to-differential conversion. An ideal method of applying differential drive to the AD7356 is to use a differential amplifier, such as the AD8138. The AD8138 can be used as a single-ended-to-differential amplifier or as a differential-to-differential amplifier. It also provides common-mode level shifting. Figure 1 shows how the AD8138 can be used as a single-ended-to-differential amplifier in a dc-coupled application. The positive and negative outputs of the AD8138 are connected to the respective inputs on the ADC through a pair of series resistors to minimize the loading effects of the switched capacitor inputs of the ADC. The architecture of the AD8138 results in outputs that are very highly balanced over a wide frequency range without requiring tightly matched external components. The single-ended-to-differential gain of the circuit in Figure 1 is equal to RF/RG, where RF = RF1 = RF2 and RG = RG1 = RG2.

Figure 1. AD8138 as a DC-Coupled, Single-Ended-to-Differential Converter Driving the AD7356 Differential Inputs (Simplified Schematic: Decoupling and All Connections Not Shown)

If the analog inputs source being used has zero impedance, all four resistors (RG1, RG2, RF1, and RF2) should be the same as is shown in Figure 1. If the source has a 50 Ω impedance and a 50 Ω termination, for example, increase the value of RG2 by 25 Ω to balance this parallel impedance on the input and thus ensure that both the positive and negative analog inputs have the same gain. This also requires a small increase in RF1 and RF2 to compensate for the gain loss caused by increasing RG1 and RG2. Complete analysis for the terminated source condition is found in the ADIsimDiffAmp interactive design tool and in the MT-076 Tutorial.

The AD7356 requires a driver that has a very fast settling time due to the very short acquisition time required achieving 5 MSPS throughput with a serial interface. The track-and-hold amplifier on the front end of the AD7356 enters track mode on the rising edge of the 13th SCLK period during a conversion. The ADC driver must settle before the track-and-hold returns to hold (38 ns later for 5 MSPS throughput on the AD7356 using an 80 MHz SCLK). The AD8138 has a specified 16 ns settling time that satisfies this requirement.

The voltage applied to the VOCM pin of the AD8138 sets up the common-mode voltage. In Figure 1, VOCM is connected to 1.024 V, which is a divided version of the internal 2.048 V reference on the AD7356. If the on-chip 2.048 V reference on the AD7356 is to be used elsewhere in a system (as illustrated in Figure 1), the output from REFA or REFB must first be buffered. The OP177 features the highest precision performance of any op amp currently available and is a perfect choice for a reference buffer.

Note that, in Figure 1, the AD8138 operates on dual 5 V supplies whereas the AD7356 is specified for power supply voltages of 2.25 V to 3.6 V. Care must be taken to ensure that the maximum input voltage limits of the AD7356 are not exceeded during transient or power-on conditions (see MT-036 Tutorial). In addition, the circuit must be constructed on a multilayer printed circuit board (PCB) with a large area ground plane. Proper layout, grounding, and decoupling techniques must be used to achieve optimum performance (see MT-031 Tutorial, MT-101 Tutorial, and the AD7356 evaluation board layout).

COMMON VARIATIONS

The OP07D, an ultralow offset voltage op amp, is a lower cost alternative to the OP177. It offers similar performance with the exception of the offset voltage specification. Alternatively, the AD8628 or the AD8638 offers very high precision with very low drift with time and temperature.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
AD7356 Differential Input, Dual, Simultaneous Sampling, 5 MSPS, 12-Bit, SAR ADC AD7356BRUZ AD7356YRUZ
AD8138 Low Distortion Differential ADC Driver AD8138SRMZ-EP-R7 AD8138ARMZ AD8138ARZ
AD8638 16 V Auto-Zero, Rail-to-Rail Output Operational Amplifier AD8638ARJZ-REEL7 AD8638ARZ
OP07D Ultralow Offset Voltage Operational Amplifier OP07DRZ OP07DNZ
OP177 Precision Op Amp

To obtain samples of this part, please contact ADI

content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close