CN0026: Precision, Unipolar, Inverting Conversion Using the AD5547/AD5557 DAC

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 09/2010 (pdf, 90 kB)
Benefits & Features
  • 14-/16-bit current to voltage conversion
  • Inverting unipolar output
    Applications: 
  • Programmable Logic Controllers/ Distributed Control Systems
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Connectivity Options
This circuit supports 3rd party connectivity.

CIRCUIT FUNCTION AND BENEFITS

This circuit provides precision, unipolar, inverting data conversion using the AD5547/AD5557 current output DAC with the ADR03 precision reference and AD8628 operational amplifier (op amp). This circuit provides accurate, low noise, high speed output voltage capability and is well suited for process control, automatic test equipment, and digital calibration applications.

Figure 1. Unipolar 2-Quadrant Multiplying Mode, VOUT = 0 V to –VREF (Simplified Schematic)

CIRCUIT DESCRIPTION

The AD5547/AD5557 are dual-channel, precision 16-/14-bit, multiplying, low power, current output, parallel input digital-to-analog converters. They operate from a single 2.7 V to 5.5 V supply with ±15 V multiplying references for 4-quadrant outputs. Built-in 4-quadrant resistors facilitate the resistance matching and temperature tracking that minimize the number of components needed for multiquadrant applications.

This circuit uses the ADR03, which is a highly accuracy, high stability, 2.5 V precision voltage reference. As voltage reference temperature coefficient and long-term drift are primary considerations for applications requiring high precision conversion, this device is an ideal candidate.

An op amp is used in the current-to-voltage (I-V) stage of this circuit. An op amp’s bias current and offset voltage are both important selection criteria for use with precision current output DACs. Therefore, this circuit employs the AD8628 auto-zero op amp, which has ultralow offset voltage (1 μV typical) and bias current (30 pA typical). The compensation capacitor, C7, is optimized to compensate for the external output capacitance of the DAC.

Note that the AD8628 has rail-to-rail input and output stages, but the output can only come within a few millivolts of either rail depending on load current. For the circuit shown, the output can swing from –2.5 V to approximately –1 mV.

The input offset voltage of the op amp is multiplied by the variable noise gain (due to the code-dependent output resistance of the DAC) of the circuit. A change in this noise gain between two adjacent digital codes produces a step change in the output voltage due to the amplifier’s input offset voltage. This output voltage change is superimposed on the desired change in output between the two codes and gives rise to a differential linearity error, which, if large enough, could cause the DAC to be nonmonotonic. In general, the input offset voltage should be a fraction of an LSB to ensure monotonic behavior when stepping through codes. For the ADR03 and the AD5547, the LSB size is

The input offset voltage of the AD8628 auto-zero op amp is typically 1 μV, which is negligible compared to the LSB size.

The input bias current of an op amp also generates an offset at the voltage output as a result of the bias current flowing through the feedback resistor, RFB. In the case of the AD8628, the input bias current is only 30 pA typical, which flowing through the RFB resistor (10 kΩ typical), produces an error of only 0.3 μV.

The AD5547/AD5557 DAC architecture uses a current-steering R-2R ladder design that requires an external reference and op-amp to convert to an output voltage. VOUT can be calculated for the AD5547 using the equation

where D is the decimal equivalent of the input code. VOUT can be calculated for the AD5557 using the equation

where D is the decimal equivalent of the input code.

COMMON VARIATIONS

For multichannel applications, the AD8629 is a dual version of the AD8628. The AD8605 is another excellent op amp candidate for the I-V conversion circuit. It also has a low offset voltage and low bias current. The ADR01 and ADR02 are other low noise references available from the same reference family as the ADR03. Other low noise references that would be suitable are the ADR441 and ADR445 products. The size of the reference input voltage is restricted by the rail-to-rail voltage of the op amp selected.

These circuits can also be used as a variable gain element by utilizing the multiplying bandwidth nature of the R-2R structure of the AD5547/AD5557 DAC. In this configuration, remove the external precision reference and apply the signal to be multiplied to the reference input pins of the DAC.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
AD5547 Dual Current Output, Parallel Input, 16-Bit Multiplying DACs with 4-Quadrant Resistors AD5547CRUZ AD5547BRUZ
AD5557 Dual Current Output, Parallel Input, 14-Bit Multiplying DACs with 4-Quadrant Resistors AD5557CRUZ
AD8605 Precision, Low Noise, CMOS, RRIO Op Amp (single) AD8605ACBZ-REEL7 AD8605ARTZ-REEL7
AD8628 Zero-Drift, Single-Supply, RRIO Op Amp AD8628ARZ AD8628ARTZ-REEL7 AD8628AUJZ-REEL7
AD8629 Zero Drift, Single-Supply, R/R, Input/Output Operational Amplifier AD8629ARMZ AD8629ARZ
ADR03 Ultracompact, Precision 2.5 V Voltage Reference ADR03AKSZ-REEL7 ADR03ARZ ADR03AUJZ-REEL7
content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close