ANALOG DEVICES’ 16-BIT DUAL ADC USES HALF THE POWER OF COMPETING DATA CONVERTERS, WHILE ACHIEVING LOWEST NOISE PERFORMANCE IN ITS CLASS

- ADI’s AD9650 analog-to-digital converter lowers energy use and simplifies board layout in high-performance medical imaging and industrial data acquisition systems.
The AD9650, a low-power, low-noise ADC designed for high-performance data acquisition systems.

Norwood, MA (07/29/2010) - Analog Devices, Inc. (ADI) announced today a dual 16-bit 105 MSPS (mega samples per second), low-power, low-noise, ADC (analog-to-digital converter) designed for high-performance data acquisition systems in medical imaging, industrial, spectrum analysis, multimode radio and radar applications. The AD9650 ADC consumes 328-mW per channel, which is half the power per channel of competing data converters while achieving an industry best SNR (signal-to-noise ratio) figure of 82 dBFS and SFDR (spurious-free dynamic range) performance of 90 dBc with a 30 MHz input. For more information, visit http://www.analog.com/pr/AD9650.

“In the medical imaging arena, our customers are constantly striving for higher resolution image capture that improves patient diagnostics,” said Patrick O’Doherty, vice president for the Healthcare Group, Analog Devices. “The AD9650 helps our customers achieve that goal by allowing medical equipment designers to increase imaging channel densities while still maintaining system-critical low noise and power requirements.”

Available in a compact 9 mm x 9 mm package, the AD9650 provides flexibility for engineers using proprietary differential inputs at frequencies up to 300 MHz and includes an on-chip dither option for improved SFDR performance with low signal level analog inputs. The new ADC is pin-compatible with ADI’s previously release dual ADCs, including the AD9268 16-bit 125 MSPS, AD9251 14-bit 80 MSPS and the AD9269 16-bit 80 MSPS, allowing system engineers to raise the performance of their data acquisition systems without changing the board layout.

The AD9650 operates from a single 1.8 V supply and a separate digital output driver supply, accommodating 1.8 V CMOS or LVDS outputs. The AD9650 is also available in speed grade options of 80 MSPS, 65 MSPS and 25 MSPS.

AD9650 Key Features

  • 105/80/65/25 MSPS Sample Rates
  • 16-Bit Resolution
  • SNR: 82 dBFS at 30 MHz and 105 MSPS
  • SFDR: 90 dBc at 30 MHz and 105 MSPS
  • Low power: 328 mW/channel at 105 MSPS
  • Optional on-chip dither
  • 1.8-V analog supply operation

As part of a complete signal chain, the AD9650 can be used with amplifiers, VGAs and clock drivers such as the ADL5562 3.3 GHz ultralow -distortion RF/IF differential amplifier, ADA4937-2 ultralow -distortion differential ADC driver, AD8372 programmable dual VGA, AD9510 clock distribution IC and AD9520 CMOS output clock generator with integrated VCO.

Pricing and Availability

Product Sample
Availability
Resolution
(Bits)
Data Rate
(MSPS)
Price Each
Per 1,000
Packaging
AD9650-105 NOW 16 105 $122.50 64-lead LFCSP
AD9650-80 NOW 16 80 $105.00 64-lead LFCSP
AD9650-65 NOW 16 65 $87.50 64-lead LFCSP
AD9650-25 NOW 16 25 $52.50 64-lead LFCSP

More Information, Samples and Tools

Data Converters: Bridging the Analog and Digital Worlds
More designers turn to Analog Devices than any other supplier for the high-performance conversion technology required to bridge the analog and digital worlds in today’s myriad electronic systems. With the industry’s leading portfolio of ADCs (analog-to-digital converters) and DACs (digital-to-analog converters), Analog Devices’ converter products feature the right combination of sampling rates and accuracy with low noise, power, and price and small package size required by industrial, medical, automotive, communications, and consumer electronics. Online evaluation tools help customers quickly validate, select, and design in the optimal data converters to reduce design complexity, development schedules, and bill-of-material costs. To view ADI’s ADC selection guide, visit http://www.analog.com/ADC-Search. For ADC drivers, visit http://www.analog.com/ADC-Drivers. To view ADI’s DAC selection guide, visit http://www.analog.com/DAC-Search.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Subscribe to ADI’s News Feed.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

Editor's Contact Information:

Bob Olson
781/937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close