Sensors Expo 2010 , Rosemont, IL (06/01/2010) - At the Sensors Expo 2010 conference, Analog Devices, Inc. (ADI) is demonstrating how high-performance signal processing technology is being applied to a new generation of sensor and sensor interface ICs for medical, automotive, industrial, instrumentation, and consumer applications. Visit ADI at booth #901 in the Donald E. Stephens Convention Center, Rosemont, IL June 8 - 9, 2010. For more information about the exhibition, please visit: www.analog.com/sensorsexpo.
A Preview of ADI’s Sensors Expo Demos
Here is a brief overview of what visitors to ADI’s Sensors Expo booth will see, hear and experience:
New products being introduced include:
ADI will also be presenting two papers:
For More Information
For more information or to set up an interview with ADI representatives before or during the Sensors Expo show – or to schedule a personal demonstration of ADI technologies at the show – please contact Howard Wisniowski at 781-937-1517 or howard.wisniowski@analog.com.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
CapTouch, iMEMS and iSensor are registered trademarks of Analog Devices, Inc.
Subscribe to ADI’s News Feed.
Follow ADI on Twitter at http://www.twitter.com/ADI_News.
Howard Wisniowski
781/937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved