| Isolating the Key Data (or Lunching With a Mermaid and Pickled Herring) | |
| Q. There is a fault in my CMOS multiplexer...? | |
|
It was in Copenhagen. I had been discussing an analog electronics course with a professor from the University of Copenhagen and we decided to walk through Kastellet to see the Little Mermaid on her rock before having lunch on the quayside at Nyhaven in the oldest part of the harbor. As we walked Lars told me that Karen, one of his graduate students, was having accuracy troubles making measurements on three channels with one analog-to-digital converter (ADC).
If there are three channels there is usually a fourth not being used so I told him I could probably cure the problem on that information alone. We telephoned the student and told her to ground all unused multiplexer (MUX) inputs and outputs, and retest her system.
Unconnected channels on CMOS switches and MUXes, whether on a separate chip or part of a multi-input ADC, can pick up signals from stray electrostatic fields and inject them into the substrate of the chip, turning on spurious substrate deviceseven if the unconnected channel is disabled. These devices' leakage can degrade the performance of the active channel or channels, or even of an ADC which shares the chip.
In the past the effect might be so large as to trigger a parasitic thyristor across the supplies and destroy the device, but modern CMOS processes are mostly protected against such catastrophes, but not against more subtle degradations of accuracy. "Fault-protected" switches and MUXes are far less vulnerable to such effects, too, but not totally immune and by no means are all MUXes fault-protected as the protection circuitry increases chip size and, as a result, cost.
It is therefore essential that all inputs and outputs of a CMOS switch or MUX, even one integrated into an ADC, be connected to a potential somewhere between its supplies. Generally this means grounding all unused inputs and outputs, but sometimes leakage and/or capacitive crosstalk can better be minimized by connecting unused pins to a signal or a power supply.
By the time Lars and I had consumed a Tuborg and a plate of marinated herring, and had waved goodbye to the mermaid, Karen had called us back to report that her system was working perfectly.
| Download this article (pdf 1,892,352 bytes) | back to top |
| James Bryant Offers Intrigue, Interest and Technological Troubleshooting Ideas... engineer, applications manager, philosopher, humorist, columnist and radio ham (G4CLF), only a man with such an eclectic dossier could make the often drab world of semiconductors come to life with such color and imagination. | ![]() |
For More Information:
If It's Not Being Used, Ground It!
Winning the Battle Against Latch-Up in Analog CMOS Switches
Analog Dialogue, Ask the Applications Engineer, Switches and Multiplexers
Bus Switches for Speed, Safety, and Efficiency: What They Are and What You Should Know about Them
An IC Amplifier User's Guide to Decoupling, Grounding, and Making Things Go Right for a Change
Grounding for Low- and High-Frequency Circuits
Useful Analog Devices Links:
© 1995 - Analog Devices, Inc. All Rights Reserved