RAQs
Digital processing does not always rule (Or, what makes an analog engineer laugh?)
Q. Why recommend analog signal processing when digital systems are so cheap and powerful?

Analog/Digital



A.   Because sometimes analog signal processing is even cheaper, and can do things that digital processing cannot. Sales of analog signal processing circuits support this. The Science Museum in South Kensington, London, was founded in Queen Victoria's reign. Although it is imaginatively run and well worth a visit, it is scarcely renowned for its humor. On a recent visit to their computer science area, however, I laughed so much, and so loudly, that I barely escaped arrest for disorderly behavior. The cause of my uncontrolled mirth was a glass case labeled, "Obsolete Analog Computing Technology," containing, among other things, an AD534 analog multiplier. ADI has been making this device for more than 30 years, and it continues to generate substantial sales revenue.


In fact there are a number of operations where analog processing has clear advantages over digital. Digital multiplication is simple and cheap, but if the original data and the required output are both analog, the cost and complexity of analog-to-digital converters (ADCs) and digital-to-analog converters (DACs) to convert from analog to digital – and back again – often exceed those of an analog multiplier. Also, the digital propagation delay may be too great for a high-speed system.


In addition, it may be more efficient to process the analog signals before the ADC, even if digital data is required. An example is ac power measurement. If the signal to be measured is a simple 50 or 60 Hz sine wave and the load is resistive, then the measurement is simple. But if the signal is more complex, the load is reactive, or the frequency is higher, then it is necessary to over-sample both the voltage and the current in the load to determine the actual power, increasing the demands on converters and processor. An analog multiplier driven by the voltage and current in the load has an output proportional to instantaneous power, which may be integrated and sampled quite slowly.


Even if we are only interested in the root-mean-square (rms) voltage of a complex waveform, analog rms computation works at several gigahertz – 100 times faster than an over-sampled digital system.


And, of course, the dynamic range of the highest resolution ADC is 20 or 30 dB less than that of an analog logarithmic amplifier. So there are still a number of areas where analog signal processing offers substantial cost and performance advantages over digital.

Download this article (pdf, 28,672 bytes) back to top

James Bryant Offers Intrigue, Interest and Technological Troubleshooting Ideas... engineer, applications manager, philosopher, humorist, columnist and radio ham (G4CLF), only a man with such an eclectic dossier could make the often drab world of semiconductors come to life with such color and imagination. James Bryant


For More Information:

Analog Computation in the Digital Age (pdf, 1,261,568 bytes)


Multipliers
Analog Multiplier Product Table
AN-212 AD834 Multiplier (pdf)
AN-213 AD539 Multiplier (pdf)
AN-216 AD834 VCA (pdf)
AN-255 AD539 VCA (pdf)
AN-304 AD538 Analog Computer (pdf)
AN-309 Fast VCAs (pdf)
AD534 Data Sheet (pdf)
AD633 Data Sheet (pdf)
AD734 Data Sheet (pdf)
AD834 Data Sheet (pdf)
AD835 Data Sheet (pdf)

RMS-DC Converters (LDF)
RMS-DC Application Guide (zip)
AN-268 RMS-DC Converters (pdf)
AN-269 Extending RMS-DC Dynamic Range (pdf)

RMS-DC Converters (VHF)
AN-653 RF RMS Detectors (pdf)
AN-691 LF Operation of HF (RMS) Detectors (pdf)

Log Amps
AN-304 AD538 Analog Computer (pdf)


Useful Analog Devices Links:

Analog Dialogue

Webcasts from Analog Devices

Sign up for Analog Devices eNewsletters

Analog Devices Homepage

back to top

Send Feedback X
content here.
content here.

Send Feedback

Close