POLYPHASE ACTIVE ENERGY METERING IC WITH SERIAL INTERFACE

The ADE7754 provides Active Energy, RMS values, temperature measurement and Apparent Energy information via a serial interface. This documentation describes the ADE7754 evaluation kit Hardware and Software functionality. The evaluation board (watt-hour meter) is configured via the parallel port of a PC. The data interface between the evaluation board and the PC is fully isolated. Windows™ based software is provided with the evaluation board which allows it to be quickly configured as an energy meter.

The ADE7754/ADE7758 evaluation board and this documentation, together with the ADE7754 data sheet, provide a complete evaluation platform for the ADE7754. The ADE7754 evaluation board can be configured by setting jumpers.

The evaluation board has been designed so that the ADE7754 can be evaluated in the end application, i.e., Watt-Hour Meter. Using the appropriate transducers on the current channel (e.g., CT) the evaluation board can be connected to a test bench or high voltage (240 V rms) test circuit. On-board resistor dividers networks provide the attenuation for the line voltages. This application note also describes how the current transducers should be connected for the best performance. The evaluation board requires two external 5 V power supplies (one is required for isolation purposes) and the appropriate current transducers.

Documentation

Technical notes are available in Adobe Acrobat Portable Document Format (PDF).
To download the technical notes, select the links below:

Software

To download the software, select the link below:

Send Feedback X
content here.
content here.

Send Feedback

Close