XILINX AND ANALOG DEVICES ACHIEVE JEDEC JESD204B INTEROPERABILITY

Milestone set to accelerate widespread adoption of All Programmable devices and ADI’s data converters in communications equipment

San Jose, Calif.,  (09/24/2013) - Xilinx, Inc. (NASDAQ: XLNX) and Analog Devices, Inc. (NASDAQ: ADI) today announced that they have achieved JESD204B interoperability between Xilinx JESD204 LogiCORE™ IP in the Kintex®-7 FPGA and the ADI AD9250 analog-to-digital high-speed data converter. Achieving JESD204B interoperability between logic and data converter devices is a significant milestone in promoting the widespread adoption of this new technology.

Transition to the high-speed transceiver based JESD204B standard opens up significant upsides for improving system performance in communications equipment. JESD204B offers manufacturers numerous advantages, including higher level system integration, deterministic latency capability, easier multi-channel synchronization, smaller and lower-cost device packages, reduced PCB complexity and cost, and better system modularization.

"By demonstrating JESD204B interoperability, Xilinx and ADI have shown leadership in this important new standard," said Harpinder Matharu, senior product manager, Xilinx Communications Business Unit. “Working together, Xilinx and ADI can enable manufacturers to take advantage of JESD204B to accelerate time-to-market for their new products by shortening development time, reducing system test effort, and minimizing development issues."

"Interoperability testing between Xilinx FPGAs and ADI data converters is a significant milestone for analog and digital designers worldwide and it will reinforce industry confidence in this emerging high-speed converter interface. The results confirm that off-the-shelf ADI JESD204B data converters and Xilinx FPGAs work together seamlessly," said Dave Babicz, director, Global Alliances, Analog Devices. "ADI’s portfolio includes the clocks, amplifiers and the other components, tools and software needed to successfully implement a JESD204B-based data converter-to-FPGA design, and together, ADI and Xilinx provide a complete and verified solution."

Developed by the JEDEC standards organization, the new JESD204B specification overcomes connectivity limitations between the logic device and the multiple data converter devices used in multi-mode wireless radios, wideband backhaul modems, ultrasound monitors and other high performance equipment. JESD204B eliminates the connectivity bottleneck, complexity and improves system performance while lowering cost.

The joint interoperability lab testing successfully validated JESD204B subclass 0 and subclass 1 (deterministic latency) functionality by running a comprehensive set of tests between the Xilinx Kintex-7 XC7K325T FPGA and ADI’s AD9250 device.

Xilinx JESD204 LogiCORE IP is the industry’s first JESD204B soft IP that supports continuous line rates from 1 Gb/s to 12.5 Gb/s on 1, 2, 3, 4, 5, 6, 7, or 8 lanes using GTX or GTH transceivers in Zynq®-7000, Kintex-7 and Virtex®-7 28nm devices and GTP transceivers in the 28nm Artix®-7 FPGA family. Xilinx JESD204B IP can be configured as a transmitter or receiver and supports transceiver sharing between a transmitter and receiver link.

Pricing and Availability

Xilinx JESD204 IP is now available for free evaluation at

http://www.xilinx.com/products/intellectual-property/EF-DI-JESD204.htm. For more information on Analog Devices AD9250 visit http://www.analog.com/AD9250, and for details on Analog Devices JESD204 read the survival guide at http://www.analog.com/static/imported-files/tech_articles/JESD204B-Survival-Guide.pdf

About Xilinx

Xilinx is the world’s leading provider of All Programmable FPGAs, SoCs and 3D ICs. These industry-leading devices are coupled with a next-generation design environment and IP to serve a broad range of customer needs, from programmable logic to programmable systems integration. For more information, visit www.xilinx.com.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

© Copyright 2013 Xilinx, Inc. Xilinx, the Xilinx logo, Artix, ISE, Kintex, Spartan, Virtex, Zynq, Vivado and other designated brands included herein are trademarks of Xilinx in the United States and other countries. All other trademarks are the property of their respective owners.

Follow ADI on Twitter.

Subscribe to ADI’s News Feed.

Editor's Contact Information:

Bob Olson
781-937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close