Norwood, MA (03/21/2012) - Analog Devices, Inc., (ADI) a global leader in high-performance semiconductors for signal processing applications, today introduced a single-chip energy measurement AFE (analog front end) that monitors the energy consumption and power quality of up to six electrical circuits. The ADE7816 energy measurement AFE is designed for data center power distribution units, energy monitoring and management systems, and multi-channel electricity meters. Able to measure one voltage and up to six current channels, the new AFE provides high-accuracy energy usage and power quality data for each circuit. Since it interfaces to standard microcontrollers, the ADE7816 energy measurement AFE is specifically suited for applications that require more processor flexibility and peripheral options than is offered by fixed-configuration SOC (system-on-chip) devices. Additionally, multiple ADE7816 energy measurement AFEs can interface with a single application processor resulting in scalable and cost-effective solutions.
| Product | Sample Availability | Full-Volume Production | Price Each in 1,000 Quantities | Package |
|---|---|---|---|---|
| ADE7816 | Now | Now | $6.35 | 40-lead LFCSP (lead frame chip scale package) |
With more than 350 million energy meters using ADI’s technology deployed worldwide, Analog Devices has delivered more energy measurement solutions than any other semiconductor company. Superior in quality, reliability, and performance, Analog Devices’ energy-metering ICs combine ADCs (analog-to-digital converters) with fixed-function DSPs (digital signal processors) to perform critical measurements, while providing unparalleled functionality and ease-of-use. Analog Devices offers a broad range of semiconductor solutions that solve design challenges in every aspect of metering systems, including energy measurement; data and power management; user interface; and RF, GSM/GPRS, and power-line carrier communication solutions. For more information about ADI’s energy measurement products, visit http://www.analog.com/pr/Energy-Measurement. For more information about ADI’s energy solutions for renewable energy generation, transmission and distribution, and metering applications, visit www.analog.com/energy.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Linda Kincaid
781-937-1472
linda.kincaid@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved