INDUSTRY’S FIRST OCTAL ULTRASOUND RECEIVER WITH DIGITAL I/Q DEMODULATOR AND DECIMATION FILTER REDUCES PROCESSOR OVERHEAD IN ULTRASOUND SYSTEMS

Analog Devices’ AD9670 octal ultrasound receiver captures and conditions ultrasound RF signals to ease FPGA processing burden in cart-based and portable ultrasound equipment.
AD9670

Norwood, MA (07/23/2012) - Analog Devices, Inc. (NASDAQ: ADI), the leading provider of data-conversion technology and longtime collaborator with the medical imaging industry, today introduced the industry’s first octal (eight-channel) ultrasound receiver with on-chip digital I/Q demodulation and decimation filtering. Because of the embedded demodulation and decimation feature, ADI’s AD9670 is the first ultrasound receiver able to condition eight channels of data from RF to a baseband frequency, reducing the processing load on the system FPGA (field-programmable gate array) by at least 50 percent compared to other receivers. The AD9670 also integrates a low-noise amplifier, variable gain amplifier, anti-aliasing filter, and a 14-bit, A/D converter with the industry’s highest sample rate (125 MSPS) and best SNR (signal-to-noise ratio) performance (75 dB) for enhanced ultrasound image quality. The new octal receiver is the latest addition to Analog Devices’ award winning ultrasound receiver portfolio and is designed for mid- to high-end portable and cart-based ultrasound systems.

The integrated digital I/Q demodulator, programmable-oscillator and 16-tap FIR (finite-impulse response) decimation filter of the AD9670 reduce the FPGA’s data bandwidth requirements, allowing designers to use less expensive processors or reallocate processing bandwidth to other system functions. The new receiver also provides a continuous wave (CW) processing path with an analog I/Q demodulator that has harmonic rejection to the 13th order, which allows designers to reduce the number of filter components to lower system cost, reduce design complexity, and improve signal sensitivity. The CW-mode output dynamic range is more than 160 dBc/ √Hz per channel.

Additionally, the AD9670 octal receiver’s 30-MHz anti-aliasing filter frequency and 125-MSPS A/D converter sample rate combine to yield SNR performance that is 3-dB higher than competing devices. The 14-bit A/D converter also features a programmable clock, data alignment, and programmable digital test pattern generation, including built-in fixed and pseudo random patterns and custom user-defined test patterns, entered via a serial port interface. Total power is 130-mW per channel, while an eight-channel low-noise amplifier reduces input-referred noise to just 0.78 nV/√Hz typical at 5 MHz (gain = 21.3 dB).

“By introducing the first octal ultrasound receiver with digital demodulation and decimation filtering, we are able to minimize the data I/O and throughput rates and place less stress on the system processor,” said Pat O’Doherty, vice president, healthcare segment, Analog Devices. “At the same time, by extending the anti-aliasing filter frequency range and maintaining a high A/D converter sample rate, we are continuing to help medical and industrial ultrasound equipment manufacturers meet the trend toward higher frequency probes and superior image quality.”

AD9670 Octal Ultrasound Receiver Key Features

  • Digital I/Q demodulator with programmable oscillator
  • FIR decimation filter
    • 16 taps per decimation factor
    • Maximum decimation of 32
  • 14-bit, 125-MSPS A/D converter
    • SNR: 75 dB
  • 8-channel LNA, VGA, AAF, ADC
  • Low power:
    • 130-mW/channel @ 40 MSPS in TGC (time gain compensation) mode
    • 55 mW/channel in CW mode
  • Noise: 0.78 nV/√Hz typical at 5 MHz (gain = 21.3 dB)
  • Harmonic rejection to 13th order on CW-Doppler signals


Availability, Pricing and Complementary Components

The AD9670 octal receiver with integrated digital demodulation and decimation filtering is pin-similar to ADI’s AD9278 and AD9279 octal receivers, allowing designers to upgrade cart-based and portable ultrasound equipment designs using a common PCB board layout.

Product Sample Availability Full Production Price each per 1k units Packaging
AD9670 August 2012 October 2012 $69.00 144-ball 10 mm x 10 mm BGA

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue/

Editor's Contact Information:

Edie Kramer
(781) 937-1734

edie.kramer@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close