HIGH-SPEED A/D CONVERTERS FEATURE MORE CHANNELS, LOWER POWER AND SMALLER PACKAGE SIZE

Analog Devices Introduces Highly Integrated Octal and Quad ADCs for Demanding Medical Imaging and Communications Applications
AD9257_9637_9253_9633

Norwood, MA (11/10/2011) - Analog Devices Inc. (ADI), a global leader in high-performance signal processing technology, announced today the addition of four high-speed A/D data converters to its market-leading data converter product portfolio. The two octal- and two quad-channel converters are designed for medical imaging and communications applications where the combination of high channel density, low power and small size provide systems engineers with greater design flexibility and lower per-channel cost for data conversion.

The AD9257 14-bit and AD9637 12-bit octal A/D converters each integrate eight A/D converters into one package and feature 40 percent lower power per channel than other discrete octal converters. Analog Devices today also introduced the AD9253 14-bit and AD9633 12-bit quad A/D converters in 48-lead chip-scale packages that are more than 10 percent smaller than competing devices.

Data Conversion for Medical Imaging

All of the new converters support the higher channel densities of MRI (magnetic resonance imaging) systems, medical ultrasound and other high-end imaging applications, such as industrial visual inspection systems and non-destructive ultrasound. The AD9253 14-bit and AD9633 12-bit quad A/D converters are offered in a non-magnetic package and can be used safely within the magnetic field of an MRI system. This allows the converters to be placed closer to the signal of interest, which can increase the quality of image resolution and image throughput while reducing the overall component count.

Complementary components for these high-speed converters include the AD8334 quad, ultralow noise VGA (variable gain amplifier) for ultrasound applications.

Data Conversion for Communications

The new octal and quad A/D converters are also suited to MIMO-based (multiple-input, multiple-output) radios, 3G infrastructure equipment and other wireless communications applications.

The ADL5202 variable gain wide bandwidth amplifier, AD8376 ultralow distortion IF dual VGA and ADA4937 ultralow distortion differential ADC driver work well with these high-speed converters in communications applications.

Key High Speed A/D Converter Features

  • Low ADC core power
  • Serial LVDS (ANSI-644, default)
  • Low power, reduced output swing option (similar IEEE 1596.3)
  • Data and frame clock outputs
  • Operates on a single 1.8-V power supply
  • 650-MHz full-power analog bandwidth
  • 2-V p-p input voltage range
  • Serial port control
  • Specified over the industrial temperature range of -40°C to +85°C

Pricing and Availability

Product Sample Availability Full Production Signal-to-Noise Ratio Sample Rates (MSPS) Price Each In 1,000 Quantities Packaging
AD9257 14-bit octal NOW Now 75.7 dBFS 65
40
$71.40
$46.65
64-lead LFCSP 9 mm x 9 mm
AD9637 12-bit octal Now Now 71.5 dBFS 80
40
$56.95
$40.46
64-lead LFCSP 9 mm x 9 mm
AD9253 14-bit quad Now Now 75.3 dBFS 125
105
80
$117
$100
$63
48-lead LFCSP 7 mm x 7 mm
AD9633 12-bit quad Now Now 71.8 dBFS 125
105
80
$68.51
$57.80
$44.20
48-lead LFCSP 7 mm x 7 mm
Find additional high-speed converters at http://www.analog.com/en/analog-to-digital-converters/products/index.html.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

To subscribe to ADI's News Feed http://www.analog.com/en/homepage/news.xml

Follow ADI on Twitter at http://www.twitter.com/ADI_News

Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/subscribe.html

EngineerZone is trademark of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners.

Editor's Contact Information:

Bob Olson
(781) 937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close