ANALOG DEVICES TO HOST ‘NAME THAT BEER’ DEMONSTRATION USING SPECTROMETER TECHNOLOGY FROM WASATCH PHOTONICS AT ELECTRONICA 2012

At ADI’s booth (Hall A4, Stand 159) Wasatch will identify the signature spectrum of 10 brands of beer using a Raman spectrometer incorporating ADI’s A/D converter technology.

MUNICH, Germany  (11/05/2012) - Analog Devices, Inc. (ADI) is teaming up with Wasatch Photonics, Inc. at electronica 2012 (November 13-16) to stage a “Name That Beer” demonstration using the Wasatch Photonics Stroker 785L Raman Spectrometer. Incorporating ADI’s A/D converter technology, the compact Raman laser spectrometer will distinguish from among 10 brands of German beer by reading the signature spectrum of each. The demonstration will be held at the Analog Devices booth (Hall A4 Stand 159). The Stroker 785L combines a ƒ/1.3 spectrometer using a free-space VPH (volume phase holographic) grating, a stabilized 785-nm laser, and a scientific CCD camera that integrates ADI’s precision A/D converter technology.

“The Stroker 785L can identify substances by optically probing the inherent molecular vibrational fingerprints through measurement of the laser-induced amplitude and frequency shift of the scattered light. This compact system can be used in pharmaceutical, narcotic and explosives identification in real time – and from a safe distance,” said Scott Norton, VP Engineering at Wasatch Photonics. “This demonstration offers engineers an example of how laboratory-based performance can be achieved in a compact form factor by combining high-quality parts and innovation in electrical, optical and mechanical engineering.”

About Wasatch Photonics’ Stroker 785L Raman Spectrometer with 785 nm Laser

The Wasatch Photonics’ Stroker 785L combines Wasatch’s Stroker ƒ/1.3 Spectrometer technology with its proprietary free space VPH grating, a customized high-performance CCD camera that integrates ADI’s AD7980 16-Bit, 1 MSPS PulSAR® A/D Data Converter, and a stabilized 785 nm laser package, to deliver the highest throughput in a miniature Raman spectrometer on the market. The front end optical module matches the ƒ/1.3 spectrometer input to maintain maximum efficiency. High performance hard coated filters are used to maximize transmission and minimize Rayleigh scattering. A 120mW 785 nm laser is TEC and VBG (volume Bragg grating) stabilized resulting in ultra-stable performance over time and temperature.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Follow ADI on Twitter

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Bob Olson
781-937-1666

bob.olson@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close