PULSAR® ANALOG-TO-DIGITAL CONVERTER EVALUATION KIT

Introduction

EVAL-CED1Z Software | EVAL-CONTROL BRD3Z Software | NEW! PulSAR Parallel Port Tools | User's Guides

The PulSAR evaluation tools are suited for testing and evaluating ADI's line of high resolution successive approximation register (SAR), charge redistribution, analog to digital converters ranging from 14-bits to 18-bits. The evaluation tools usually consist of the device specific evaluation board (i.e. EVAL-AD7621CBZ), a capture board (EVAL-CED1Z) and a PC where an executable version of software is run. These tools can be used to measure the converters DC and AC performances in both time and frequency domains. The PulSAR Evaluation kit is ideal for:

  • Quick evaluation of the PulSAR ADC with the evaluation software
  • Bread boarding for final hardware configuration
  • Use the board in standalone to debug final system
  • Developing a specific software application using Labview

Currently, there exist two data capture boards; the USB based EVAL-CED1Z and parallel port based EVAL-CONTROL BRDxZ (x = 2 or 3). Many of the products are supported by both capture boards however it is recommended to use the USB based CED board when possible as there exists issues with parallel ports on PCs.

PulSAR Evaluation Board/USB Converter Evaluation and Development Capture Board

Evaluation Board/USB Converter Evaluation and Development Capture Board (CED)


Software and Documentation for the Converter Evaluation and Development Board (EVAL-CED1Z)

PulSAR to EVAL-CED1Z Evaluation Software Version 1.7 (zip, 123 MB)

CED1Z (Converter Evaluation and Development Board) (pdf, 1.44 MB)

View Ordering Information


PulSAR Evaluation Board/Evaluation Control Board (EVAL-CONTROL BRDxZ), Parallel Port Based Capture Board

EVAL-CONTROL BRDxZ



Software and Documentation for the Evaluation Controller Board (EVAL-CONTROL BRD3Z)

PulSAR to EVAL-CONTROL BRDxZ Evaluation Software Version 6.1 (zip, 110 MB)

Controller for Precision Converter Evaluation/Demonstration Boards (pdf, 412 kB)

Using a DC Supply for Powering the Eval Control Board3

back to top


NEW! PulSAR Parallel Port Tools

Since PC manufacturers configure the parallel port(s) differently, the following user guide sheds some light on specific configurations for PulSAR Evaluation boards. PortTest is a useful program for determining the PC parallel port settings as described in the User Guide.

PulSAR to ECB User Guide (pdf, 447 kB)

Parallel Port Test (zip, 52.1 MB)


Select the specific documentation for the PulSAR Evaluation boards from the following table:

back to top

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close