Complete Monolithic 8-Bit, 10-µs A/D Converter

AD670 is Fully μP-Compatible, Accepts Low-Level Differential Analog Signals; Completely Self-Contained, It Operates from +5-Volt Computer Supplies

The AD670 "ADCPORT", the near-ideal 8-bit ADC, is a complete, microprocessor-compatible easy-to-use a/d converter on a single monolithic chip. A successive-approximation device, it contains its own buffer amplifier, voltage reference, d/a converter, latching comparator, successive-approximation register, 3-state output latches, and control logic. Read full article



Authors

Generic_Author_image

Doug Grant

Generic_Author_image

Diane Heerema

Doug Mercer

Doug Mercer

Doug Mercer received his B.S.E.E. degree from Rensselaer Polytechnic Institute (RPI) in 1977. Since joining Analog Devices in 1977, he has contributed directly or indirectly to more than 30 data converter products and he holds 13 patents. He was appointed to the position of ADI Fellow in 1995. In 2009, he transitioned from full-time work and has continued consulting at ADI as a Fellow Emeritus contributing to the Active Learning Program. In 2016 he was named Engineer in Residence within the ECSE department at RPI.