content here.
content here.

ANALOG DEVICES EXPANDS PORTFOLIO OF HIGH-SPEED ULTRA-LOW-NOISE OPERATIONAL AMPLIFIERS

The ADA4898’s unique combination of speed and precision offers designers maximized dynamic range for 16- and 18-bit precision instrumentation applications.
ADA4898

Norwood, MA (04/23/2008) - Analog Devices, Inc. ( ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced the ADA4898, the latest addition to its portfolio of low-noise operational amplifiers (op amps). Following the success of the ADA4899 and AD8099 operational amplifiers, the ADA4898 offers designers a unique blend of low distortion, low noise, and high speed for applications that also require high precision. Designed to work with Analog Devices’ precision data converters, including the AD7631 and AD7634, the ADA4898 is especially suited for radar-based collision avoidance, medical instrumentation and other 16-bit and 18-bit precision instrumentation applications.

“Analog Devices continues to lead the industry in offering low-noise amplifier products. The ADA4898 is the next op amp to use the common-mode linearized input that ADI pioneered with the AD8099,” said Jim Doscher, product line director for High Speed Linear Products at Analog Devices. “The ADA4898 achieves unprecedented low ‘1/f’ and broadband noise for a high-speed amplifier.”

About the ADA4898
The ADA4898 unity gain stable op amp offers design engineers ultra-low broadband noise (<1 nV/rt Hz), 1/f noise of 1.2 nV/rt Hz at 10 Hz, low distortion (¬–110 dBc at 500 kHz), and dc precision that optimizes the performance of analog-to-digital converters (ADCs). Particularly suited for 16- and 18-bit systems, the ADA4898 features high speed (–3 dB bandwidth of 70 MHz, at G=+1) and high slew rate (40 V/µs), providing the optimal combination of amplifier speed and precision. The ADA4898 has a wide supply range of from ±5 V to ±15 V.

Availability and Pricing
The ADA4898-1 single is now available in full production quantities in an 8-lead SOIC (small outline integrated circuit) package and is rated to operate over the extended industrial temperature range of –40°C to +125°C. A dual version will be available later this year. The ADA4898-1 is priced at $1.89 in 1,000-unit quantities. For more information, visit http://www.analog.com/pr/lownoiseamps.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Linda Kincaid
781-937-1472

linda.kincaid@analog.com