Webcast: Noise Optimization in Sensor Signal Conditioning Circuits (Part I & II)
View Part 1
There have been many papers and presentations on the topic of noise and still the term is used broadly with some level of confusion. Some engineers think of an amplifier's DC errors such as Vos, Ib as noise but others consider it to include AC parameters such as current noise and voltage noise density. Other typical questions include: What are noise types and their source in amplifiers and voltage references? How does noise behave with time, temperature and other conditions? How do we calculate the overall noise of a circuit? How can we optimize a circuit for best noise performance? This first part of a two-part series will explore the noise topic in detail and provide tips and answers to these types of questions.
View Part 2
This is the second part of a two-part series that explores the topic of signal noise in detail. The first session covered the types, sources, characteristics, and analysis techniques of noise, and introduced a low-noise design process. In this session, our expert will step through this entire design process and demonstrate how to manage noise to meet required signal chain performance objectives. Design "Do's" and "Don'ts" as well as a number of circuit optimization techniques will be presented.
For a complete list of ADI's available Webcasts, please visit the Webcast Library.
Presenter:
Reza Moghimi
Applications Engineering Manager,
Analog Devices, Inc.
Reza Moghimi has been with ADI since 1989 serving as test, product, project and applications engineering manager. He graduated from San Jose State University (SJSU) with a BSEE in 1984 and received his MBA in 1990. He has written numerous articles and design ideas for electronic trade publications, several of which have been highlighted as “the Best of Design Ideas”.