Material Declarations
This search allows entry of one or more ADI catalog part numbers which will return a listing of the following: product and package information, RoHS high temperature information, component weight, data on RoHS materials, and RoHS replacement parts as applicable. The results will also provide data on other materials of concern such as antimony and bromine. The results will be presented in a downloadable spreadsheet. You may request a search of up to 100 part numbers at one time.Glossary
ADI F/G Part Number. | The orderable ADI complete exact part number. Example:AD640BP. |
MCV | Maximum concentration value = upper concentration limit, as defined by ADI. |
No Data | Independent lab test results not available. |
Not Used | Not used or contained in the product. |
Package Type | Jedec package designator |
High Temperature Compatible | Compatible at 255+5/-0°C (260°C) peak reflow temperature. |
MSL Rating (per J-STD-020) | Moisture Sensitivity Level rating. |
Peak Reflow Temperature |
Maximum allowable temperature during reflow of component |
RoHs Replacement ADI F/G Part Number |
The orderable RoHS compatible ADI part number for the non RoHS compatible part. |
European Union Exemptions (E) | Parts that have been deemed RoHS compliant and falling under a EU RoHS exemption |
Moisture Sensitivity Level information for legacy Linear products. (PDF)
RoHS Compliance
European and other RoHS regulations restrict the use of four heavy metals (lead, mercury, cadmium, and hexavalent chromium) and two brominated flame retardants (polybrominated diphenyl ethers and polybrominated biphenyls) in electrical and electronic devices. ADI provides products that allow our customers to be compliant with RoHS regulations. For more information on ADI's RoHS compliance program, see Analog Devices ROHS Compliance Information (pdf).
ADI's RoHS Position Statement (pdf)
Analog Devices evaluation boards are specifically designed for the purpose of research and development and are made available on a business-to-business basis and are therefore excluded from the scope of the RoHS 2 Directive.
EU REACH
REACH is the Regulation (EC) No 1907/2006 of the European Parliament and of the Council of 18 December 2006 concerning the Registration, Evaluation, Authorization and Restriction of Chemicals. It came into force on 1 June 2007. As the REACH List of Substances of Very High Concern (SVHC) is updated by the European Chemicals Agency (ECHA), ADI will provide its customers information regarding its compliance to the current revision of the SVHC list. ADI’s REACH compliance position statement is provided in the link below. For product specific requests for REACH certifications, please contact your regional support center. Please provide your contact information, company and country in your request.
ADI’s EU REACH Position Statementwww.analog.com/en/support/technical-support
Other Position Statements
- Dimethyl fumarate (“DMF”) Statement (pdf)
- Ozone Depleting Substance Statement (pdf)
- PFOS PFOA Statement (pdf)
- Red Phosphorus Statement (pdf)
For additional information on Analog Devices’ Environmental, Health & Safety Management please visit www.analog.com/en/about-adi/sustainability/environmental-health-safety
Procedure for Return of ADI Evaluation Boards
In accordance with requirements of Waste Electrical and Electronic Equipment – WEEE Directive. This return procedure can be used for evaluation boards containing Pb or RoHS-compliant boards.
- ADI customers in the EU should contact the local sales office to arrange for pick up of evaluation boards for disposal.
- For Eval Board shipments received from a Distributor, customers should return boards to the Distributor directly.
- Evaluation Board WEEE returns should not be mixed with returns of semiconductor components.
- No credits or replacements will be issued.
- ADI will advise customer of the return order number, which customer is asked to reference on the outside of shipping boxes and paperwork.
-
Information that will be required to complete the pick up:
- Date shipment will be ready for collection.
- Number of cartons.
- Weight.
- Contact person & telephone number.
- ADI will forward customer a preprinted waybill which should be handed to the driver on collection, advising them that their local transportation depot will arrange pick up.