Press Release

Contact John Hamburger
Contact Doug Dickinson

High Efficiency N-Channel Switching Surge Stopper Protects Against 150V Transients

Jul 26 2018 - Norwood, MA
  • LTC7862_300x300

    Analog Devices announces the Power by Linear LTC7862, a high efficiency switching surge stopper with overvoltage and overcurrent protection for high availability systems. The LTC7862 drives an N-channel power MOSFET stage. During normal operation the LTC7862 passes the input voltage through to the output with minimal conduction loss. When an input overvoltage condition occurs, the LTC7862 starts switching as a high efficiency DC/DC regulator, protecting critical downstream components by limiting the output voltage and current.



    The LTC7862 builds on popular linear surge stoppers such as the LTC4363 by offering high efficiency switching protection to extend output current capability and reduce power loss during transients and faults. Supply voltages surge when the load current changes abruptly in long inductive power busses. The situation is aggravated in automotive applications by the energy stored in the alternator’s inductance, causing an elevated and extended voltage surge during a load dump. The power handling capability of a surge stopper is limited by the power lost in the protection circuit. In a linear surge stopper, the power capability is determined by the size of the pass MOSFET, while in a switching surge stopper the power capability is determined by conversion efficiency. Due to its lower power loss, a switching surge stopper can operate through longer input voltage surges at higher output current than a linear solution.


    The LTC7862 has an input voltage operating range of 4V to 140V, 150V abs max. An external fault timer capacitor configures the limited time spent in overvoltage mode and keeps the switching surge stopper below a safe peak operating temperature when power loss is at its highest levels. The fault timer saves system cost and size by allowing component selection to be optimized for normal mode rather than overvoltage transient and fault conditions.


    In MIL-STD-1275 applications the LTC7862 protects devices operating from a 28V vehicle power bus, where this bus voltage can reach as high as 100V and last up to 500ms. The LTC7862 also fits into industrial, avionics, and automotive power, including ISO 7637.


    The LTC7862 is available in 20-Lead 4mm × 5mm QFN and TSSOP packages. Three temperature grades are available, with operation from –40 to 125°C for the extended and industrial grades and a high temp automotive grade of –40°C to 150°C. For more information, visit www.analog.com/LTC7862.


    Summary of Features :LTC7862


    • VOUT Clamp Stops High Voltage Input Surges
    • 100% Duty Cycle Pass-Through Mode During Normal Operation
    • Switches During Overvoltage or Overcurrent Transients, Faults & During Start-Up
    • High Efficiency Switching Enables Long Duration Surge Protection 
    • Wide VIN Range: 4V to 140V (150V Abs Max) 
    • Adjustable Output Voltage Clamp Up to 60V 
    • Adjustable Output Overcurrent Protection 
    • RSENSE or Inductor DCR Current Sensing
    • Power Inductor Reduces Input EMI in Normal Mode 
    • Adjustable Soft-Start for Inrush Current Limiting
    • MIL-STD-1275 & ISO7637 Compatible

    Pricing & Availability
    Product Production Availability Price Each Per 1,000 Packages
    LTC7862 Now Starts at $3.40 20-Lead 4mm × 5mm QFN & TSSOP
  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue


    All registered trademarks and trademarks are the property of their respective owners.

  • Editor's Contact Information
Stay Informed