Press Release

Contact Linda Kincaid

Analog Devices’ SigmaStudio 4.0 Delivers Improved Audio Graphical Programming and Advanced Voice Processing Algorithms

Apr 3 2018 - Norwood, MA
  • Analog Devices, Inc. (ADI) today introduced a new version of its audio graphical development tool. SigmaStudio 4.0 includes new features and enhancements including more intuitive user interface controls, cross-application support, and inter-process communication designed to simplify advanced audio signal processing designs for automotive, consumer, professional audio, installation, and industrial applications.


    Download SigmaStudio 4.0: www.analog.com/sigmastudio

    Cross-application support enables SigmaStudio control from other design engineering environments, such as Python™, MATLAB®, LabVIEW, or any dotnet-based application. Inter-process communication allows SigmaStudio to send information packets to one or more supported remote processors (e.g. TCP/IP).


    SigmaStudio 4.0 offers users increased speed for design cycles by using indirect generic function calls instead of direct memory mapping to avoid recompiling uC host code. It also enables integration of third-party algorithms into the SigmaStudio ecosystem.


    “We are thrilled to start working with the updated SigmaStudio features,” said Albert Yong, Head of Electronics and Software at Bowers and Wilkins (B&W). “With the indirect parameter access and control, and improved scripting, we are going to save time and further refine our line of products.”

  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • Read and subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/analog-dialogue.html

  • Editor's Contact Information
Stay Informed