Press Release

Contact Doug Dickinson

Stand-Alone Lead Acid Battery Balancing IC Works with up to Four 12V Batteries in Series

Jan 27 2015 - MILPITAS, CA
  • Linear Technology Corporation announces the LTC3305, a single IC, stand-alone multicell battery balancer for 12V lead acid batteries. Balancing works by absorbing charge from higher voltage batteries and transferring that charge to lower voltage batteries so that all are charged equally. Charge is transferred using a lower capacity battery that is sequentially connected across the batteries in the stack. Not only does this battery transfer charge, but the energy in the transfer battery adds to the total energy in the stack, thus increasing capacity. Included on the chip is sequencing, drive circuitry for high voltage external NFETs, voltage monitoring and protection. The LTC3305 is designed for stand-alone operation and does not require a microprocessor or other control circuitry. With the LTC3305, one battery in the stack can be replaced and quickly balanced to the remaining batteries. The LTC3305 is ideal for applications such as telecom backup systems, home battery-powered backup systems, electric vehicles and industrial lighting systems.


    The LTC3305 employs an auxiliary battery storage cell to transfer charge to or from each individual battery in the stack. A mode pin provides two operating modes: A timer mode and continuous mode. In timer mode, once the balancing operation is completed, the LTC3305 goes into a low power state for a programmed time and then periodically rebalances the batteries. In continuous mode, the balancing operation continues even after the batteries are balanced to their programmed termination voltage. Further, additional devices can be stacked to balance higher voltage series battery packs.


    The LTC3305 is offered in a thermally enhanced low profile (0.75mm) 38-lead TSSOP package. The E and I grades are specified with operating junction temperature range of –40°C to 125°C. Devices are available from stock and 1,000-piece pricing starts at $6.95. For more information, visit www.linear.com/products/LTC3305.


    Summary of Features: LTC3305


    • Single IC Balances up to Four 12V Lead Acid Batteries in Series
    • All NFET Design
    • Stackable to Balance Higher Voltage Series Battery Packs
    • Stand-Alone Operation Requires No External µP or Control Circuitry
    • Balancing Current Limited by External PTC Thermistor
    • Continuous Mode & Timer Mode
    • Programmable UV & OV Fault Thresholds
    • Programmable Termination Time & Termination Voltage
    • Thermally Enhanced 38-Lead TSSOP Package

    Stand-Alone Multicell Lead Acid Battery Balancer

    LTC3305 - PR Photo

    The USA list pricing shown is for budgetary use only. International prices may differ due to local duties, taxes, fees and exchange rates.


    Download PDF version

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed