Press Release

Contact Doug Dickinson

100V Flyback Controller Now Offered in Military –55°C to 150°C MP Grade

Mar 18 2015 - MILPITAS, CA
  • Linear Technology Corporation announces a new military MP grade version of the LT3748, a high input voltage isolated flyback DC/DC controller. This device simplifies the design of an isolated DC/DC converter by not requiring an opto-isolator, third winding or signal transformer for feedback since the output voltage is sensed from the primary-side flyback signal. The LT3748 operates over a 5V to 100V input voltage range and drives an external N-channel power MOSFET, making it well suited for a wide variety of automotive, industrial, telecom and datacom applications.


    The LT3748 operates in boundary mode, which is a variable frequency current mode control switching scheme, resulting in ±5% typical regulation over the full line, load and temperature range. Boundary mode also permits the use of a smaller transformer compared to equivalent continuous conduction mode designs. The output voltage is easily set by two external resistors and the transformer turns ratio. Several off-the-shelf transformers are identified in the data sheet that can be used for numerous applications. The high level of integration and the use of boundary mode operation results in a simple, clean application solution to the traditionally tough problem of isolated power delivery.


    Additional features include an on-board low drop regulator for IC power, programmable soft start, undervoltage lockout, adjustable current limit and output voltage temperature compensation.


    The LT3748MP operating junction temperature is from –55°C to 150°C and the device is housed in a MSOP-16 package with 4 pins removed for additional high voltage pin spacing. The 1,000 piece price starts at $9.25 each. For more information, visit www.linear.com/product/LT3748.


    Summary of Features: LT3748MP


    • –55°C to 150°C Junction Temperature Operation
    • VIN Range from 5V to 100V
    • No Opto-Isolator, Transformer or Third Winding Required for Feedback
    • Drives External N-channel Power MOSFET
    • Current Mode Control
    • Boundary Mode Operation
    • VOUT Set with Two External Resistors
    • Off-the-Shelf Transformers
    • Programmable Soft-Start
    • Programmable Under Voltage Lockout
    • Output Voltage Temperature Compensation

    100V Isolated Flyback Operates Over –55°C to 150°C

    LT3748MP PR Image

    The USA list pricing shown is for budgetary use only. International prices may differ due to local duties, taxes, fees and exchange rates.


    Download PDF version

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed