Press Release

Contact Doug Dickinson

9V to 72V Ideal Diode Bridge Controller Now Specified from -55°C to 125°C for Military & Automotive Applications

Mar 5 2014 - MILPITAS, CA
  • Linear Technology Corporation announces the automotive (H-grade) and high reliability military (MP-grade) versions of the LT4320, an ideal diode bridge controller for 9V to 72V systems. The LT4320 replaces a full-wave diode bridge rectifier with a low loss N-channel MOSFET bridge to reduce the power and voltage losses by a factor of ten or more. Power supply size is reduced as the enhanced power efficiency eliminates bulky heat sinks. Low voltage applications benefit from the extra margin afforded by saving the two diode drops inherent in diode bridges. Compared to the traditional alternative, the MOSFET bridge enables a rectifier design that is highly space- and power-efficient. The H- and MP-grade versions are guaranteed over the –40°C to 125°C and –55°C to 125°C temperature ranges, respectively. More information on Linear Technology’s MP-grade flow is available at /media/en/quality-documentation/mpgrade.pdf.


    The LT4320 switch control smoothly turns on the appropriate two MOSFETs, while keeping the other two off to prevent reverse currents. An integrated charge pump provides the gate drive for the external low on-resistance N-channel MOSFETs without requiring external capacitors. The choice of MOSFETs offers the greatest flexibility in power levels ranging from one to thousands of watts.


    The LT4320 is available in two options: the LT4320 is designed for DC to 60Hz voltage rectification, whereas the LT4320-1 is optimized for DC to 600Hz by doubling the topside source-drain regulation voltage. The H-grade is offered in 8-pin DFN (3mm × 3mm) and PDIP packages and a 12-lead MSOP package with enhanced high-voltage pin spacing, while the MP-grade is offered in the 12-lead MSOP package only. 1,000-piece H- and MP-grade pricing starts at $3.45 and $8.85 each, respectively. Device samples and evaluation circuit boards are available online or from your local Linear Technology sales office. For more information, www.linear.com/product/LT4320.


    Summary of Features: LT4320H/MP


    • Low Loss Replacement for Diode Bridge Rectifier
    • Minimizes Heat to Ease Thermal Design
    • Maximizes Power Efficiency & Available Voltage
    • 9V to 72V, DC to 600Hz Operation
    • Controls Four N-Channel MOSFETs
    • 1.5mA Quiescent Current
    • –40°C to +125°C Guaranteed Junction Temperature Range (H-Grade)
    • –55°C to +125°C Guaranteed Junction Temperature Range (MP-Grade)
    • 8-Pin DFN (3mm × 3mm), 8-Lead PDIP & 12-Lead MSOP Packages

    –55°C to 125°C Rated Active Bridge Rectifier Conserves Power & Voltage


    Download PDF version

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed