Press Release

Contact Grainne Murphy Market Manager

Analog Devices Releases Two Dual A/D Converters with Lowest Power/Highest Linearity Combination Available

AD7902, AD7903 PulSAR® A/D converters provide robust, flexible, simultaneous sampling solutions for industrial applications.

Jun 19 2014 - Norwood, MA
  • Analog Devices, Inc. (NASDAQ:ADI) introduced today two 16-bit, 1-MSPS A/D converters with pseudo differential and differential input options. The AD7902 dual pseudo differential and AD7903 dual differential PulSAR® A/D converters enable simultaneous or independent signal chain implementation to provide two sampling solutions in one package. Each A/D converter consumes 12 mW @ 1 MSPS, which is 70 percent less power than the closest competitor. Power consumption is scaled depending on throughput speed to address thermal dissipation challenges in dense data acquisition system designs. The A/D converters feature up to +/-0.5 LSB and 94 dB SNR for exceptional accuracy and precision making them ideally suited to a wide range of high performance multichannel applications including I/Q demodulation, motor and power control, automated test equipment, data acquisition and medical instrumentation.

    • Download AD7902 and AD7903 data sheet, order samples and evaluation boards
    • Connect with engineers and ADI product experts on EngineerZone™, an online technical support community

    Both A/D converters incorporate a versatile serial interface port and are implemented as physically-isolated devices allowing for a robust signal chain design with functional safety considerations in mind. The physical isolation also allows verification and backup measurements enabling useful end-system fault detection.


    Pricing and Availability 

    Product
    Sample Availability/Full Production
     Resolution
    Input   Price Each Per 1,000
     Packaging
     AD7902
     NOW
     16-Bit
     Pseudo Differential
     $15
     20-lead QSOP
     AD7903
     NOW
     16-Bit
     Pseudo Differential
     $15
     20-lead QSOP

     

     

     

     

     
    The A/D converters can be designed into circuits for data acquisition applications with ADI’s ADA4841-1, ADA4941-1 or ADA4940 low-noise, low-distortion, rail-to-rail output amplifiers, the ADP7104 low-noise LDO and ADR4525 voltage reference series.

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • PulSAR is a registered trademark and EngineerZone is a trademark of Analog Devices, Inc.


    To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe


  • Editor's Contact Information
Stay Informed