Press Release

Contact Jim Surber Editor

Analog Devices Unveils a 16-Bit, 310 MSPS, Dual A/D Converter Providing Industry-leading Noise and Linearity Performance Over a Wide Input Range

The AD9652 A/D converter’s -156 dBFS noise floor and 85 dBFS large signal spurious-free dynamic range allow low level signals to be captured in cluttered spectral environments.

May 27 2014 - Norwood, MA
  • Analog Devices, Inc. (ADI), a global leader in high-performance signal processing technology and the data converter market share leader, today introduced the AD9652, 16-bit, 310 MSPS dual A/D converter, designed to support the more demanding high-speed signal processing applications that require exceptional linearity and noise performance over a wide input frequency range. The AD9652 can digitize up to 155 MHz of signal bandwidth and provides an analog input bandwidth of 650 MHz. The high performance input buffer and 16 bit A/D converter core provide the high linearity and noise performance necessary to detect and isolate weak signals in the presence of large signals, blockers, and spectral clutter. This can simplify the signal chain and move more of the system control, configuration, and tuning into the software domain. Target applications for the AD9652 include multi-mode, multi-band, communications receivers, RADAR, and RF test equipment.

    The AD9652 supports input clock frequencies up to 1.24 GHz with an integer 1-to-8 clock divider used to generate the A/D converter sample clock. A duty cycle stabilizer is provided to compensate for variations in the ADC clock duty cycle. The 16-bit output data (with an over-range bit) from each A/D converter’s is interleaved onto a single LVDS output port along with a double data rate clock. Programming for setup and control are accomplished using a 3-wire SPI-compatible serial interface.

    • View the AD9652 A/D converter product page, order samples, and download the data sheet
    • Get support at ADI’s EngineerZone™ online technical support community
    • Buy and evaluate today: Digi-Key Corp. and Mouser Electronics are stocking inventory of evaluation boards.

    AD9652 Features

    • High Dynamic Range for IF sampling:
      • SNR = 73.7 dBFS at 170 MHz (AIN = -1 dBFS)
      • SFDR= 85 dBFS at 170 MHz (AIN = −1 dBFS)
    • Excellent noise spectral density (NSD) performance:
      • −156.7 dBFS/Hz input noise
      • −157.6 dBFS/Hz for small signal, <-6dBFS at 70 MHz
    • 90 dB channel isolation/crosstalk
    • On-Chip Dithering (improves small signal linearity)
    • Analog Bandwidth of 650 MHz

    The AD9652’s dual A/D converter cores feature a multistage, pipelined architecture with integrated output error correction logic. A high performance on-chip buffer and internal voltage reference is used to simplify the interface to external driving circuitry while preserving exceptional dynamic performance.

    Pricing, Availability and Complementary Products

    Product

     Sample Availability

     Production Release

     Resolution(Bits)

     Channels

     Sample Rate(MSPS)

     Price Each In 1,000 Quantities

     Packaging

     AD9652-310

     Now

     Now

     16

     1

     310

     $231.25

     144-CSPBGA

     AD9652-310EBZ

     

     Now

     

     

     

     $395

     


    Complementary ADI signal chain components include the ADA4938-2 dual ultra-low distortion A/D converter driver amplifier, and the ADL5565 high performance differential amplifier optimized for RF and IF applications.

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • EngineerZone is a trademark of Analog Devices, Inc.

    To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

  • Editor's Contact Information
Stay Informed