Press Release

Contact Doug Dickinson

Cable Drop Compensator Corrects Remote Load Regulation Errors without Sense Wires

Apr 17 2013 - MILPITAS, CA
  • Linear Technology Corporation announces the LT6110 cable drop compensator, a new device that improves voltage regulation at remote loads without the need for Kelvin sense wires. The LT6110, a new component for the designer, has been architected for use with most types of voltage regulators and can provide several volts of load regulation compensation.


    The LT6110 will compensate for the voltage drop due to resistance in a wire, circuit board trace or cable and can improve regulation at the load by a factor of 10. It operates with supply voltages that range from 2V to 50V, making it suitable for high power USB, Power over Ethernet (PoE), remote instrumentation and remote industrial applications. The LT6110 reduces costs by eliminating sense wires which may be prone to misconnection or damage and it makes load regulation independent of wire size or length.


    The LT6110 operates by measuring the load current with a sense resistor and injecting current into the existing regulator’s feedback loop to raise the output voltage. It is designed to work with standard feedback circuits, as well as new “current source” reference devices such as the LT3080. For load currents less than 3A, the internal 20mΩ sense resistor simplifies the design. Wide bandwidth achieves fast transient compensation of load steps, and in most cases the savings in wire and labor are more than the cost of the LT6110.


    According to Robert Dobkin, Vice President of Engineering and CTO for Linear Technology, “The LT6110 is a unique power supply component that gives designers a new degree of freedom by improving voltage regulations without the need of sense wires.”


    The LT6110 is fully specified for operation from –40°C to 125°C and is offered in SOT23 and 2mm × 2mm DFN packages. It is now available, priced starting at $1.29 each in 1,000-piece quantities. For more information, visit www.linear.com/product/LT6110.


    Summary of Features: LT6110


    • Operates with Almost All Existing Voltage Regulators
    • Correction Set with a Single Resistor
    • High Side Current Sensing:
      • Integrated 20mΩ Sense Resistor for up to 3A
      • Ability to Use an External Sense Resistor
    • 300µV Maximum Input Offset Voltage
    • Output Current Accuracy of 1% Maximum
    • 30µA Maximum Supply Current
    • 2V to 50V Supply Range
    • Fully Specified from –40°C to 125°C
    • Available in Low Profile (1mm) ThinSOT & 2mm × 2mm DFN Packages

    Improve Voltage Regulation at Remote Loads without Sense Wires

    LT6110 PR Image

    Download PDF version

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed